Skip to main content
trevor1
Associate III
May 8, 2009
Question

Hardware CRC on byte buffer

Posted on May 08, 2009 at 10:26

Hardware CRC on byte buffer

    This topic has been closed for replies.

    4 replies

    bob239955
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 12:36

    I am wondering if once again the documentaion is wrong and that

    CRC_DR = CRC_DR + CRC_IDR

    (32bit) = (32bit) + (8bit)

    (where + means crc)

    might be worth a try. 8-)

    Otherwise whats the point of the CRC_IDR register?

    trevor1
    trevor1Author
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 12:36

    The hardware CRC works on 4 bytes at a time (CRC->DR is a 32 bit register).

    How do you CRC a buffer that contains a number of bytes not divisible by 4

    i.e. what do you do with the last 1, 2 or 3 bytes?

    E.g.

    unsigned char buffer[5] = { 1, 2, 3, 4, 5 }; // CRC ????

    Regards

    Trevor

    ericbrocke9
    Associate
    May 17, 2011
    Posted on May 17, 2011 at 12:36

    Dit you see that 0x4C11DB7 is the bit-revered version of 0xEDB88320?

    The implementation is common on hardware designs (fi. FPGA) but from C-code it is not. You have to bit-reverse the data before you write to the CRC_DR register. The result of the CRC calculation should be bit-reversed and negated (^ 0xFFFFFFFF).

    See also

    http://www.st.com/mcu/forums-cat-7171-23.html

    about this subject.

    It seems that there is a design flaw about the CRC calculation unit. I think that CRC_IDR register originally was intended to calculate the CRC on a single byte but they could not get it right on the implementation. It would be nice if they fix it on new devices.

    trevor1
    trevor1Author
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 12:36

    Hi bobz,

    I wondered that also.

    Anyway I'm not going to use the hardware CRC now as it uses the wrong polynomial -- 0x4C11DB7 and I want to use 0xEDB88320. It's a shame you cannot set the polynomial.

    The reason I looked at hardware CRC was to reduce the size of my booloader i.e. not have to store the 1k CRC table in code. I got round this by generating the the CRC table in RAM rather than defining it in code.

    Regards

    Trevor