Skip to main content
cable gu
Associate II
Nov 23, 2018 7:37 AM UTC
Question

Hardfault on IAP jump to APP

Hi guys,

I have use the stm32f105 to do a job on the IAP jump tp APP, and normally it works fine, but latest day, I have to disable the USB code on the APP code, then use the flash download demonstrator to download the APP, it runs OK, and then re-power on the device, APP run into hard fault at once.

And I have print the CFSR=0x8200, HFSR=0x40000000, BFAR=0x5548535f(this value seems not right). I can not use BFAR to find the error place. So any one could give some suggestion?

    This topic has been closed for replies.

    10 replies

    u_2man
    Associate II
    Nov 23, 2018 7:47 AM UTC

    Hi..

    Try to de-init RCC and SysTick before jump to application

      HAL_RCC_DeInit();

      SysTick->CTRL =0;

      SysTick ->LOAD =0;

      SysTick->VAL=0;

      JumpAddress = *(__IO uint32_t*) (APPLICATION_ADDRESS + 4);

      JumpToApplication = (pFunction) JumpAddress;

      /* Initialize user application's Stack Pointer */

      //SCB->VTOR = APPLICATION_ADDRESS;

      __set_MSP(*(__IO uint32_t*) APPLICATION_ADDRESS);

      JumpToApplication();

    Usman

    cable gu
    cable guAuthor
    Associate II
    Nov 23, 2018 8:53 AM UTC

    Hi Usman,

    Thanks for giving the suggestion, and it still goes into the hard fault, and the test code as below:

    if (((*(__IO uint32_t*)ApplicationAddress) & 0x2FFE0000 ) == 0x20000000)

    {

    //__disable_interrupt();

    __set_PRIMASK(1);

    HAL_RCC_DeInit();

      SysTick->CTRL =0;

      SysTick ->LOAD =0;

    SysTick->VAL=0;

    //HAL_DeInit();

    /* Move the 4 bytes to APP address */

    JumpAddress = *(__IO uint32_t*) (ApplicationAddress + 4);

    /* Point to the APP entry address */

    Jump_To_Application = (pFunction) JumpAddress;

    /* Reset the top of the stack point address */

    __set_MSP(*(__IO uint32_t*) ApplicationAddress);

    /* Jump to the reset function */

    Jump_To_Application();

    }

    and now, I think the IAP code does not recycle the source, and the main in IAP is below:

    int main(void)

    {

    HAL_Init();

    /* Configure the system clock */

    SystemClock_Config();

    /* Initialize all configured peripherals */

    MX_GPIO_Init();

    JumpToApp();

    /* Infinite loop */

    /* USER CODE BEGIN WHILE */

    while (1)

    {

    /* USER CODE END WHILE */

    /* USER CODE BEGIN 3 */

    }

    /* USER CODE END 3 */

    }

    Maybe there is still some interrupt running?

    u_2man
    Associate II
    Nov 23, 2018 9:23 AM UTC

    Have you shift the interrupt vector on your application code?

    cable gu
    cable guAuthor
    Associate II
    Nov 23, 2018 9:31 AM UTC

    Yes, I did the shift. And normally, the IAP and APP runs OK. This hard fault appear just when I disable the USB host function in APP. So it confused me.

    /* #define VECT_TAB_SRAM */

    #define VECT_TAB_OFFSET 0x00006000U /*!< Vector Table base offset field. 

    Tesla DeLorean
    Guru
    Nov 23, 2018 12:00 PM UTC

    Looks to be loading a pointer with the content of an ASCII string.

    ​

    Really should be looking at LR and PC values and understanding the specific code that is faulting. Look at .MAP file or listing file.​

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    cable gu
    cable guAuthor
    Associate II
    Nov 26, 2018 2:53 AM UTC

    Yes, I think so. Just disable the USB function and the code size reduced, so the map changed, this may related with the problem. And I am looking at the assemble code now, I hope there will be find something.

    Tesla DeLorean
    Guru
    Nov 26, 2018 3:32 AM UTC

    Make sure you have a couple of KB for the stack

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    cable gu
    cable guAuthor
    Associate II
    Nov 26, 2018 5:52 AM UTC

    Not GNU tools.

    You said that the statics not initialized means there is static variable or function?