HardFault handler asm msp/psp routine
Trying to track the cause of hardfault handler and got next problem.
MCU - STM32F302CB and i'm using eclipse with gnu mcu plugins. I'm trying to use the following code for assembly part of handler, which determines which stack is used:
__asm volatile
(
" tst lr, #4 \n"
" ite eq \n"
" mrseq r0, msp \n"
" mrsne r0, psp \n"
" ldr r1, [r0, #24] \n"
" ldr r2, handler2_address_const \n"
" bx r2 \n"
" handler2_address_const: .word prvGetRegistersFromStack \n"
);However when hardfault occurs and this piece of code is executing the program just jumps to some strange address and then stops executing. So when i execute line by line (in disassembly) it's happening on branch instruction (line 9). And in r2 there is really an address which is not valid, i mean it is not the address of prvGetRegistersFromStack, they differ.
But if i change code to something like this:
__asm volatile
(
" tst lr, #4 \n"
" ite eq \n"
" mrseq r0, msp \n"
" mrsne r0, psp \n"
" b prvGetRegistersFromStack \n"
);Then it works fine and jumps to this C function which logs stack data.
I've seen this code in a couple of articles. Exactly this code is from:
https://www.freertos.org/Debugging-Hard-Faults-On-Cortex-M-Microcontrollers.html
But it doesn't work for me, what am i missing ?