Skip to main content
demonk
Associate
October 28, 2009
Question

HardFault error when accessing DMA configuration-bits using bitbanding

  • October 28, 2009
  • 2 replies
  • 617 views
Posted on October 28, 2009 at 11:48

HardFault error when accessing DMA configuration-bits using bitbanding

    This topic has been closed for replies.

    2 replies

    tomas23
    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 13:27

    1. make sure you enable clock to (both) DMA units

    2. make sure the address calculated with your macro is correct

    3. btw. the DMA variable is initialized?

    Hard fault is a generic collector for other exceptions, enable bus fault, usage and memory fault exceptions and read the source instruction address and reason in NVIC error registers.

    [ This message was edited by: edison on 28-10-2009 16:19 ]

    demonk
    demonkAuthor
    Associate
    May 17, 2011
    Posted on May 17, 2011 at 13:27

    Good morning,

    I have a somewhat weird problem that is easy to reproduce, but I don't get the reason for it:

    Code:

    int main()

    {

    FLASH->ACR = 0x00000012;

    stm32_ClockSetup(); //Nothing fancy, HSE on, PLL on...

    BITACCESS(RCC->AHBENR)[0]=1; //DMA clock enable

    DMA->CPAR3=0xAA5500FF; //Some random address values

    DMA->CCMAR3=0x000AA000;

    DMA->CNDTR3=0x05;

    DMA->CCR3=0x00;

    DMA->CCR3|=0x02; //Set Bit 1

    DMA->CCR3|=0x01; //Set Bit 0

    }

    when I replace either of the last two lines using my BitBanding - Macro

    (BITACCESS(DMA->CCR3)[1]=1; or BITACCESS(DMA->CCR3)[0]=1; like used before to set DMA clock in RCC), I run into a hard fault error.

    Using the Keil simulator I can see in the DMA peripheral tab that the correct bits are set. But on the real hardware, hard fault every time.

    The calculated bit addresses are correct, I checked that.

    Did I miss something here? Can't I access these bits using bit banding? And why?

    Regards

    Benjamin