Hard Fault Unaligned Error on memory region from SDRAM
- 5 replies
- 1022 views
Hi everyone!
I have a working project based on STM32F746 with LCD, Ethernet and SDRAM(IS42S16160J-6TL) and now we are moving it to STM32H753II. I set up a FMC controller and tested whole SDRAM region with 8, 16, and 32 bit access. I use GCC.
During this migration I discovered a line of the code that always generate a HardFault error with UNALIGNED flag set. This is this line:
if (strncmp(data + i, boundary_str, 9) == 0)
from:
for (i = 0; i < len; i++)
{
if (strncmp(data + i, boundary_str, 9) == 0)
{
boundaryOffset = i + 9;
break;
}
}
data is placed in SDRAM like this:
char eth_rx_buf[MAX_LENGH] __attribute__((section (".sdram_noncached")));
and boundary_str like this:
static const char boundary_str[10] = "boundary=";
HardFault happens every time when i becomes 10.
MPU settings were copied from STM32F7 project:
/** Initializes and configures the Region and the memory to be protected
*/
MPU_InitStruct.Enable = MPU_REGION_ENABLE;
MPU_InitStruct.BaseAddress = 0xC0000000;
MPU_InitStruct.Size = MPU_REGION_SIZE_16MB;
MPU_InitStruct.AccessPermission = MPU_REGION_FULL_ACCESS;
MPU_InitStruct.IsBufferable = MPU_ACCESS_NOT_BUFFERABLE;
MPU_InitStruct.IsCacheable = MPU_ACCESS_NOT_CACHEABLE;
MPU_InitStruct.IsShareable = MPU_ACCESS_NOT_SHAREABLE;
MPU_InitStruct.Number = MPU_REGION_NUMBER3;
MPU_InitStruct.TypeExtField = MPU_TEX_LEVEL0;
MPU_InitStruct.SubRegionDisable = 0x00;
MPU_InitStruct.DisableExec = MPU_INSTRUCTION_ACCESS_DISABLE;
HAL_MPU_ConfigRegion(&MPU_InitStruct);
/** Initializes and configures the Region and the memory to be protected
*/
MPU_InitStruct.Enable = MPU_REGION_ENABLE;
MPU_InitStruct.BaseAddress = 0xC1000000;
MPU_InitStruct.Size = MPU_REGION_SIZE_16MB;
MPU_InitStruct.AccessPermission = MPU_REGION_FULL_ACCESS;
MPU_InitStruct.IsBufferable = MPU_ACCESS_NOT_BUFFERABLE;
MPU_InitStruct.IsCacheable = MPU_ACCESS_CACHEABLE;
MPU_InitStruct.IsShareable = MPU_ACCESS_NOT_SHAREABLE;
MPU_InitStruct.Number = MPU_REGION_NUMBER4;
MPU_InitStruct.TypeExtField = MPU_TEX_LEVEL1;
MPU_InitStruct.SubRegionDisable = 0x00;
MPU_InitStruct.DisableExec = MPU_INSTRUCTION_ACCESS_DISABLE;
data and boundary_str reside in 0xC0000000 part.
I have tried almost everything that I could find in Internet.
Please, give me some advice what is the cause of the HardFault. I can change this code to compare these strings one char at a time, but I want to know why it happens at all.
Thanks in advance.