Associate II
August 5, 2016
Question
Hard Fault in STM32CubeMX Generated Code
- August 5, 2016
- 1 reply
- 2225 views
Posted on August 05, 2016 at 06:07
This is an STM32CubeMX 4.16.0 generated project. The STM32CubeMX project file is attached. The processor is an STM32F373VCT6
I have a Hard Fault. Below is the call stack and register contents when the Hard Fault happened. It happens in STM32CubeMX generated code. I have suspicion it has something to do with TIM6, which is used to serve as the hardware ticker timer for FREERTOS. TIM6 was selected in an earlier version of STM32CubeMX. I no longer see where the hardware ticker timer is selected for FREERTOS. I only see that TIM6 is grayed out in Pinout tab. This function is where it happened: __STATIC_INLINE void NVIC_EnableIRQ(IRQn_Type IRQn) { NVIC->ISER[(((uint32_t)(int32_t)IRQn) >> 5UL)] = (uint32_t)(1UL << (((uint32_t)(int32_t)IRQn) & 0x1FUL)); } Any help in fixing this would be appreciated. HardFault_Handler() at Segger_HardFaultHandler.c:293 0x8006578 <signal handler called>() at 0xfffffff1 HAL_TIM_IRQHandler() at stm32f3xx_hal_tim.c:2,812 0x800d902 TIM6_DAC1_IRQHandler() at stm32f3xx_it.c:255 0x801ae24 <signal handler called>() at 0xfffffff9 NVIC_EnableIRQ() at core_cm4.h:1,628 0x8017da0 HAL_NVIC_EnableIRQ() at stm32f3xx_hal_cortex.c:237 0x8017da0 HAL_InitTick() at stm32f3xx_hal_timebase_TIM.c:74 0x801aee0 HAL_Init() at stm32f3xx_hal.c:165 0x8019de0 main() at main.c:244 0x801b588 HardFaultRegs.SavedRegs struct {...} {...} r0 volatile unsigned int 0x20006ea8 r1 volatile unsigned int 0x0 r2 volatile unsigned int 0xfffffff7 r3 volatile unsigned int 0x0 r12 volatile unsigned int 0x0 lr volatile unsigned int 0x801ae25 pc volatile unsigned int 0x800d902 psr union {...} {...} byte volatile unsigned int 0x21000046 bits struct {...} {...} IPSR unsigned int 0x46 EPSR unsigned int 0x10000 APSR unsigned int 0x4 #hard-fault-stm32-inittick()