STMicroelectronics, and all STM32 families Team wish you a happy new Year 2008 with plenty of health and success. In 2008, STM32 family lines will grow and will see an expansion of the current options with Larger packages up to 512KB Flash, 64KB SRAM and with extended features such as External Memories/Bus support, SDIO, I2S, and DAC with additional features and many new services for our customers. All the best for 2008 with STM32 ;)
We appreciate all of your interest and comments about our future microcontrollers. As this kind of information has a sensitive nature, we may not respond to this public posts in this forum. The best way to serve you is : 1)Use our online support structure at
Another question, does the the External memory Interface is compatible with Nor and Nand flash ? I would like to use both in my scanner application one for code and the other for data logging. Thank You. Magigimix[ This message was edited by: asterix.magigimix on 01-01-2008 22:46 ]
I am going to use this year the STM32 in several projects, but most important is the laser beam position sensor for the monitoring of large experimental setups in CERN accellerator experiments. The only feature which I need in addition to the STM32F103 series existing chips is DAC. Concerning I want to ask. 1. If it is planed to have DAC in small package 36 and/or 48 pin? 2. If yes, then when approximatelly I can expect to have samples? Thank you in advance, Varuzhan