Skip to main content
Associate II
Nov 7, 2024 2:46 PM UTC
Question

Half bridge, complementary outputs and dead-time insertion

I want to drive havfbridge with STM32G474. I am going to use TIMx with channel1 and channel2 to create two PWM signals, that are 180° out of phase and with the same PWM % that is limited to 0% < PWM % < 49%. Because tohose signals have max 50% duty cycle and are 180° out of phase, they cant be bot high at once. 
I already have code with multiple  __HAL_TIM_SET_COMPARE calls, but i heard about Complementary outputs.
I dont find settings for this in my Cube MX , can anyone help? Does STM32G474 have that or only STM32F series?

Here are manuals:
https://www.st.com/resource/en/reference_manual/rm0440-stm32g4-series-advanced-armbased-32bit-mcus-stmicroelectronics.pdf

And pages:
28.3.17 for timers TIM1, TIM8 and TIM20
and
30.4.14 for timers TIM15, TIM16 and TIM17

This topic has been closed for replies.

1 reply

ST Employee
Jan 8, 2025 11:02 AM UTC

Hello @Miha, 

Yes, the STM32G474 does support complementary PWM outputs. 

You can refer to the example provided in the STM32G4 Cube package: STM32CubeG4/Projects/NUCLEO-G474RE/Examples/TIM/TIM_ComplementarySignals at master · STMicroelectronics/STM32CubeG4

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.