Skip to main content
Visitor II
May 27, 2024
Question

half a USB problem on STM32F401

Hi

 

I designed a replacement pcb for a keyboard of mine with an STM32F401(RCT6).

I used the QMK framework to make a firmware which I can download via DFU perfectly fine (I also uploaded it and checked it against what I downloaded..). The PC detects the keyboard when running the firmware, but can't connect (USB errors -32 and -71). I tested the firmware on my Mode Envoy which uses the same exact chip and it work, so naive me rules out defective firmware.

Here is the link to my kicad project: https://github.com/zegonix/custom-cycle7-pcb

So far I tested the supply voltage, the reset signal and the clock as well as the usb signals. The supply voltage and reset signals seem perfect to me, the clock is a stable 12 MHz with 900 mV amplitude (can't remember the offset, but seemed reasonable) and the usb signals have a little overshoot, but seem good enough. It's only full speed (12 MHz) after all.

Does this issue seem familiar to anyone? Or any pointers?

 

Best regards,

blap

This topic has been closed for replies.

1 reply

ST Technical Moderator
September 9, 2024

Hi @blap 

 

Would you consider using a USB analyzer to trace the USB traffic?

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.Best regards,FBL