Skip to main content
LCorb.2
Associate II
April 21, 2025
Question

HAL_XSPI_Transmit timeout

MCU: STM32U5G9VJ

I am sending simple single-line commands using the HAL_XPI library and the HSPI peripheral.

Problem (See code at bottom of post):

If I use the blocking call HAL_XSPI_Transmit, I get a timeout.

if I use the DMA call HAL_XSPI_Transmit_DMA, I get a HAL_XSPI_ErrorCallback.
The OSPI peripheral is working fine, it is the HSPI only that is having this issue.

Clock Setup:

LCorb2_1-1745257208096.png

 

LCorb2_0-1745257186264.png

 

Code:

 

 HAL_StatusTypeDef status;

 XSPI_RegularCmdTypeDef sCommand = {0};

 sCommand.IOSelect = HAL_XSPI_SELECT_IO_3_0;
 sCommand.OperationType = HAL_XSPI_OPTYPE_COMMON_CFG;
 sCommand.InstructionMode = HAL_XSPI_INSTRUCTION_1_LINE;
 sCommand.InstructionWidth = HAL_XSPI_INSTRUCTION_8_BITS;
 sCommand.InstructionDTRMode = HAL_XSPI_INSTRUCTION_DTR_DISABLE;
 sCommand.Instruction = cmd;
 // Address Config
 sCommand.AddressMode = HAL_XSPI_ADDRESS_1_LINE;
 sCommand.AddressWidth = HAL_XSPI_ADDRESS_24_BITS;
 sCommand.Address = address;
 // Data Config
 sCommand.DataMode = HAL_XSPI_DATA_1_LINE;
 sCommand.DataLength = data_len;
 sCommand.DataDTRMode = HAL_XSPI_DATA_DTR_DISABLE;

 status = HAL_XSPI_Command(&hxspi1, &sCommand, HAL_XSPI_TIMEOUT_DEFAULT_VALUE);
 if (status != HAL_OK) {
 LOG_ERR("HSPI CMD Error: %d\n", status);
 Error_Handler();
 }

#define USE_DMA 0

#if USE_DMA == 1

 is_tx_done = false;

 status = HAL_XSPI_Transmit_DMA(&hxspi1, data);
 if (status != HAL_OK) {
 LOG_ERR("HSPI Error: %d\n", status);
 Error_Handler();
 }

 // wait for the previous transmission to complete
 uint64_t timeout_check = 0;
 while (!is_tx_done) {

 if (++timeout_check > (1E6)) {
 LOG_ERR("HSPI Interrupt Timeout\n");
 Error_Handler();
 }
 }

#else

 status = HAL_XSPI_Transmit(&hxspi1, data, HAL_XSPI_TIMEOUT_DEFAULT_VALUE);

 if (status != HAL_OK) {
 LOG_ERR("HSPI CMD Error: %s (%d)\n", HAL_Status_To_String(status), status);
 Error_Handler();
 }

#endif

 HAL_Delay(2);

 

This topic has been closed for replies.

3 replies

Tesla DeLorean
Guru
April 21, 2025

Are we sure this is a Timeout? Not sure clocking out data is gated on any pin state.

Is the peripheral in a busy state when you send the failing transaction?

In Memory Mapped mode?

Interrupt handlers and callbacks, and NVIC all configured?

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
LCorb.2
LCorb.2Author
Associate II
April 21, 2025

 


@Tesla DeLorean wrote:

Are we sure this is a Timeout? Not sure clocking out data is gated on any pin state.

Yes, HAL_XSPI_Transmit returns HAL_TIMEOUT.  

It flushes out the transmit data, but then it times out on the transfer complete flag check:

status = XSPI_WaitFlagStateUntilTimeout(hxspi, HAL_XSPI_FLAG_FT, SET, tickstart, Timeout);

 if (status != HAL_OK)
 {
 break;
 }

 *((__IO uint8_t *)data_reg) = *hxspi->pBuffPtr;
 hxspi->pBuffPtr++;
 hxspi->XferCount--;
 } while (hxspi->XferCount > 0U);

 if (status == HAL_OK)
 {
 /* Wait till transfer complete flag is set to go back in idle state */
 status = XSPI_WaitFlagStateUntilTimeout(hxspi, HAL_XSPI_FLAG_TC, SET, tickstart, Timeout);

 


@Tesla DeLorean wrote:

In Memory Mapped mode?

Interrupt handlers and callbacks, and NVIC all configured?


I have not called any memory map configs.  I do have the interrupts and callbacks configured, but I would not expect to need those in the blocking HAL_XSPI_Transmit call.  The HAL_XSPI_Transmit_DMA call does hit the errorcallback, so callback is being called in that configuration. 

LCorb.2
LCorb.2Author
Associate II
April 30, 2025

I think the issue was the “memory size” settings.  I had this set to 16 Bits, but when I bumped this to 16Gbits it fixed the transmit error.  This seems odd since I am not using memory-mapped mode.

Some additional questions.

Background: I am sending 640 bytes of  data with @ 100 MHz

Instruction: 1 Byte: 0x32
Address: 3 bytes

Pin settings: Very High Speed

  1. Clocks are being sent pre-chip select

    There are a series of clocks being sent before the chip select goes low.  I have a free-running clock off; why am I seeing extra clocks?

    LCorb2_11-1746047950145.png

     

  2. The first clock pulse is sometimes missing:

    Every instruction/command is 0x32.

    However, some commands seem to be missing the first clock, and shifting this command to 0x64

    Correct Instruction Bytes – first clock is at 12ns, CMD is 0x32
     
    Incorrect Instruction Byte – first clock is at 20ns, CMD is 0x64
    LCorb2_13-1746047950149.png

     

  3. Delays in the data stream when sending 640 bytes using DMA.

    The data stream has random pauses in the stream when sending 640 bytes @ 100 Mhz.  Perhaps the bus cannot keep up at this speed?

I am using DMA and enabled burst length of 64

LCorb2_15-1746047950155.png