Question
HAL_UART_Transmit_DMA
i'veA question related to transmission using DMA. i'm facing a strange situation.
- it works perfectly when i use "HAL_UART_Transmit_DMA(&huart1, TxBuf, 5);" in the main program.
- However in my project i've crated a separate file for my application program, which i include in the main program, and when i call "HAL_UART_Transmit_DMA(&huart1, TxBuf, 5);" from my application program, only first two bytes are transferred as per my data rest all bytes are corrupted.