Skip to main content
LSlat.1
Associate
Nov 13, 2020 8:31 AM UTC
Solved

HAL_TIM_PeriodElapsedCallback() refuses to trigger

Greetings

I have attempted to write an application, to toggle the LD4 LED (On PD12) on the STM32F407VGTx Discovery board. I am toggling the LED, on interrupt, when the timer overflows. I have placed the HAL_GPIO_Toggle() in the HAL_TIM_PeriodElapsedCallback() function. The LED is never be toggled. I have tried placing the Toggle function in the TIM6 IRQ handler itself and it works fine. I've also experimented with PWM recently and the HAL_OC_DelayElapsedCallback(), and the code is always executed. The Period_ElapsedCallback() function is the only problematic. Any help would be appreciated, to show where I'm going wrong.

Msp.c

void HAL_MspInit(void) 
{ 
 __HAL_RCC_SYSCFG_CLK_ENABLE();
_HAL_RCC_PWR_CLK_ENABLE();
 
HAL_NVIC_SetPriorityGrouping(NVIC_PRIORITYGROUP_4);
 
}
 
void HAL_UART_MspInit(UART_HandleTypeDef *huart)		
 {
	 GPIO_InitTypeDef GPIO_USART1;
 //1. Enable clock for usart2 peripheral and GPIOB
	 __HAL_RCC_USART1_CLK_ENABLE();
	 __HAL_RCC_GPIOB_CLK_ENABLE();
 //2. Do pin mux config(involves initialising pins for USART RX and TX)
	 GPIO_USART1.Pin = GPIO_PIN_6; //UART1 TX
	 GPIO_USART1.Mode = GPIO_MODE_AF_PP;
	 GPIO_USART1.Pull = GPIO_PULLUP;
	 GPIO_USART1.Speed = GPIO_SPEED_FREQ_LOW;
	 GPIO_USART1.Alternate = GPIO_AF7_USART1;
	 HAL_GPIO_Init(GPIOB, &GPIO_USART1);
 
	 GPIO_USART1.Pin = GPIO_PIN_7;	//UART1 RX
	 HAL_GPIO_Init(GPIOB, &GPIO_USART1);
 
	 //3. enable IRQ and set up priority (NVIC settings)
	 HAL_NVIC_EnableIRQ(USART1_IRQn);	
	 HAL_NVIC_SetPriority(USART1_IRQn, 15, 0);
 
void HAL_TIM_Base_MspInit(TIM_HandleTypeDef *tim_baseHandle){
 
	 if(tim_baseHandle->Instance==TIM6)
	 {
	 /* USER CODE BEGIN TIM6_MspInit 0 */
 
	 /* USER CODE END TIM6_MspInit 0 */
	 /* TIM6 clock enable */
	 __HAL_RCC_TIM6_CLK_ENABLE();
 
	 /* TIM6 interrupt Init */
	 HAL_NVIC_SetPriority(TIM6_DAC_IRQn, 0, 1);
	 HAL_NVIC_EnableIRQ(TIM6_DAC_IRQn);
	 /* USER CODE BEGIN TIM6_MspInit 1 */
 
	 /* USER CODE END TIM6_MspInit 1 */
	 }
 
 }
 
 void HAL_TIM_Base_MspDeInit(TIM_HandleTypeDef* tim_baseHandle)
 {
 
 if(tim_baseHandle->Instance==TIM6)
 {
 /* USER CODE BEGIN TIM6_MspDeInit 0 */
 
 /* USER CODE END TIM6_MspDeInit 0 */
 /* Peripheral clock disable */
 __HAL_RCC_TIM6_CLK_DISABLE();
 
 /* TIM6 interrupt Deinit */
 HAL_NVIC_DisableIRQ(TIM6_DAC_IRQn);
 /* USER CODE BEGIN TIM6_MspDeInit 1 */
 
 /* USER CODE END TIM6_MspDeInit 1 */
 }
 }

main.c

void UART1_Init(void);
void ErrorHandler(void);
void SystemClockConfig(void);
void GPIO_LED(void);
void TIMER6_INIT();
void HAL_IncTick();
 
UART_HandleTypeDef H_UART1 = {0};			//handle variable for the asynchronous USART2 periperhal config
TIM_HandleTypeDef tim6 = {0};
 
extern char Data[];
 
int main(void){
 
	HAL_Init();
	SystemClockConfig();
	UART1_Init();
	GPIO_LED();
	TIMER6_INIT();
 
	TIM6 -> SR = 0;
 
	while(1){}
 
	return 0;
 
}
 
void SystemClockConfig(void){
 
	RCC_OscInitTypeDef RCC_OscInitStruct = {0};
	RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
 
 
	 __HAL_RCC_PWR_CLK_ENABLE();
	 __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);
 
 
		 /** Initializes the CPU, AHB and APB busses clocks
		 */
		 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;
		 RCC_OscInitStruct.HSEState = RCC_HSE_ON;
		 RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
		 RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;
		 RCC_OscInitStruct.PLL.PLLM = 4;
		 RCC_OscInitStruct.PLL.PLLN = 168;
		 RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2;
		 RCC_OscInitStruct.PLL.PLLQ = 7;
		 if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
		 {
		 ErrorHandler();
		 }
		 /** Initializes the CPU, AHB and APB busses clocks
		 */
		 RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
		 |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
		 RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
		 RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
		 RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV4;
		 RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV2;
 
		 if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_5) != HAL_OK)
		 {
		 ErrorHandler();
		 }
 
			/**Configure the Systick
			*/
			HAL_SYSTICK_CLKSourceConfig(SYSTICK_CLKSOURCE_HCLK);
 
			/* SysTick_IRQn interrupt configuration */
			HAL_NVIC_SetPriority(SysTick_IRQn, 0, 0);
 
}
 
void UART1_Init(void){	//high level initialisation
 
	//this is done to initialise the handle to the base address of the peripheral
	H_UART1.Instance = USART1; //linking
	H_UART1.Init.BaudRate = 115200;
	H_UART1.Init.WordLength = UART_WORDLENGTH_8B;
	H_UART1.Init.StopBits = UART_STOPBITS_1;
	H_UART1.Init.Parity = UART_PARITY_NONE;
	H_UART1.Init.HwFlowCtl = UART_HWCONTROL_NONE;
	H_UART1.Init.Mode = UART_MODE_TX_RX;
	if (HAL_UART_Init(&H_UART1) != HAL_OK)//problem occured
	{
		//(HAL_OK is a keyword found in the init function, which has a structure for the status of the init after you try to initialise)
		ErrorHandler();
	}
}
 
void ErrorHandler(void){
	while(1);
}
 
 
/*
 * basic timer initialisation. always counts up
 */
void TIMER6_INIT(void){
 
	TIM_MasterConfigTypeDef sMasterConfig = {0};
 
	tim6.Instance = TIM6;
	tim6.Init.Prescaler = 8400;
	tim6.Init.CounterMode = TIM_COUNTERMODE_UP;
	tim6.Init.Period = 1000-1;
	tim6.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE;
	if(HAL_TIM_Base_Init(&tim6) == HAL_OK){
		return HAL_TIM_Base_Start_IT(&tim6);
	}
}
 
void GPIO_LED(void){
 
	GPIO_InitTypeDef gpioLED = {0};
	__HAL_RCC_GPIOD_CLK_ENABLE();
	gpioLED.Mode = GPIO_MODE_OUTPUT_PP;
	gpioLED.Pin = GPIO_PIN_12 | GPIO_PIN_13;
	gpioLED.Pull = GPIO_NOPULL;
	gpioLED.Speed = GPIO_SPEED_FREQ_LOW;
	HAL_GPIO_Init(GPIOD, &gpioLED);
 
 
 
}
 
void HAL_TIM_PeriodElaspedCallback(TIM_HandleTypeDef *timer){
	if(timer->Instance == TIM6){
	if(TIM6 -> SR & TIM_SR_UIF){
		HAL_GPIO_TogglePin(GPIOD, GPIO_PIN_12);
		TIM6->SR = ~(TIM_SR_UIF);
	}
 }
}

it.c

extern TIM_HandleTypeDef tim6;
 
extern UART_HandleTypeDef H_UART1;
 
extern char Data[50];
 
 
 
void SysTick_Handler(void){
 
 
 
	HAL_IncTick();
 
	HAL_SYSTICK_IRQHandler();
 
 
 
}
 
 
 
void TIM6_DAC_IRQHandler(void){
 
 
 
#include "main.h"
 
 
 
 
 
extern TIM_HandleTypeDef tim6;
 
extern UART_HandleTypeDef H_UART1;
 
extern char Data[50];
 
 
 
void SysTick_Handler(void){
 
 
 
	HAL_IncTick();
 
	HAL_SYSTICK_IRQHandler();
 
 
 
}
 
 
 
void TIM6_DAC_IRQHandler(void){
 
HAL_TIM_IRQHandler(&tim6);
 
}

    This topic has been closed for replies.
    waclawek.jan
    waclawek.janBest answer
    Super User
    Nov 14, 2020 9:39 AM UTC

    > HAL_TIM_PeriodElaspedCalllback

    Elasped ?

    JW

    6 replies

    TDK
    Nov 13, 2020 1:59 PM UTC

    > if(TIM6 -> SR & TIM_SR_UIF){

    The flags are cleared in HAL_TIM_IRQHandler. If it's made it to HAL_TIM_PeriodElaspedCallback, then you already know it's an update interrupt.

    Within HAL_TIM_IRQHandler:

     /* TIM Update event */
     if(__HAL_TIM_GET_FLAG(htim, TIM_FLAG_UPDATE) != RESET)
     {
     if(__HAL_TIM_GET_IT_SOURCE(htim, TIM_IT_UPDATE) !=RESET)
     {
     __HAL_TIM_CLEAR_IT(htim, TIM_IT_UPDATE);
     HAL_TIM_PeriodElapsedCallback(htim);
     }
     }

    "If you feel a post has answered your question, please click ""Accept as Solution""."
    LSlat.1
    LSlat.1Author
    Associate
    Nov 13, 2020 3:03 PM UTC

    Thank you for looking through my code.

    However, I have also tried removing the code segment, that checks if the flag has been set and the flag-reset from the TIM_PeriodElapsedCallback() and it still does not seem to work. Initially, I just checked if the instance of the timer is TIM6, and I toggled my LED, like below, which was to no avail.

    void HAL_TIM_PeriodElaspedCallback(TIM_HandleTypeDef *timer){
    	if(timer->Instance == TIM6){
    		HAL_GPIO_TogglePin(GPIOD, GPIO_PIN_12);
    	}
    }

    waclawek.jan
    waclawek.janBest answer
    Super User
    Nov 14, 2020 9:39 AM UTC

    > HAL_TIM_PeriodElaspedCalllback

    Elasped ?

    JW

    Piranha
    Principal III
    Nov 14, 2020 10:33 AM UTC

    Good catch! I wonder how do people get such errors. It seems that they use copy-paste where they shouldn't (ST's example code) and do not use it where they really should use it (function names etc.). :)

    waclawek.jan
    Super User
    Nov 15, 2020 11:48 AM UTC

    There are only two kinds of software developers: those who make this type of errors, and those who don't admit it.

    JW