Skip to main content
ABoyd.1
Associate
June 25, 2020
Question

HAL_SPI_TRANSMIT sending bits unreliably

Hello,

I'm a new new member and user of STM32 microcontrollers. I've just started using a bluepill STM32F103C8T6 microcontroller and I'm trying to set up a simple SPI communication.

At the moment I do not have slaves, only a master (the STM32), and I'm monitoring the MOSI pin with an oscilloscope. That MOSI pin is set low when inactive.

I've been trying for several days now to use the HAL_SPI_TRANSMIT function.

My code is simple:

  • libraries & function definitions
  • Running Init functions
  • DaisyChain_Init => the piece of code I'm trying to fix
  • Infinite loop with a blinking LED

I've managed to get my daisy chain function to work but for some reason (??) it only works with certain bytes. If I send 0x05, I can see the corresponding trace on my oscilloscope (00000101). If I send 0x88, I see 10001000 going through but then the MOSI pin stays high!

I have no idea why

Any help is welcome :)

#include "main.h"

#include "spi.h"

#include "gpio.h"

void SystemClock_Config(void);

void SPI1_EnableSlave(void);

void SPI1_DisableSlave(void);

void DaisyChain_Init(void);

int main(void)

{

 HAL_Init();

 SystemClock_Config();

 MX_GPIO_Init();

 MX_SPI1_Init();

 DaisyChain_Init();

 while (1)

 {

    // Turn on/off LED

    HAL_GPIO_TogglePin(BP_LED_GPIO_Port, BP_LED_Pin);

    // Delay in ms

    HAL_Delay(100);

 }

void SystemClock_Config(void)

{

 RCC_OscInitTypeDef RCC_OscInitStruct = {0};

 RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};

 /** Initializes the CPU, AHB and APB busses clocks

 */

 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;

 RCC_OscInitStruct.HSEState = RCC_HSE_ON;

 RCC_OscInitStruct.HSEPredivValue = RCC_HSE_PREDIV_DIV1;

 RCC_OscInitStruct.HSIState = RCC_HSI_ON;

 RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;

 RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;

 RCC_OscInitStruct.PLL.PLLMUL = RCC_PLL_MUL9;

 if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)

 {

   Error_Handler();

 }

 /** Initializes the CPU, AHB and APB busses clocks

 */

 RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK

                             |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;

 RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;

 RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;

 RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV2;

 RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;

 if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_2) != HAL_OK)

 {

   Error_Handler();

 }

}

void SPI1_EnableSlave()

{

   // Set slave SS pin low

   HAL_GPIO_WritePin(SPI1_CS_GPIO_Port, SPI1_CS_Pin, GPIO_PIN_RESET);

}

void SPI1_DisableSlave()

{

   // Set slave SS pin high

   HAL_GPIO_WritePin(SPI1_CS_GPIO_Port, SPI1_CS_Pin, GPIO_PIN_SET);

}

void DaisyChain_Init()

{

   uint8_t SpiOutputBuffer;

   SPI1_EnableSlave();

   SpiOutputBuffer = 0x88;

   HAL_SPI_Transmit(&hspi1, &SpiOutputBuffer, 1, 1);

   SPI1_DisableSlave();

}

This topic has been closed for replies.

4 replies

AlexKeisy
Associate II
June 25, 2020

You can connect MOSI to MISO via 1k resistor, to take null modem =) what you write that`s you will read.

ABoyd.1
ABoyd.1Author
Associate
June 25, 2020

I can try that, but the thing is I'm not even trying to read anything, I'm just looking to spit out bytes on the MOSI...

TDK
June 25, 2020

> MOSI pin is set low when inactive.

Why do you think this? MOSI doesn't have an "inactive state". It's only sampled when SCK goes high/low. There's nothing invalid about MOSI staying high or low when SCK is inactive.

"If you feel a post has answered your question, please click ""Accept as Solution""."
ABoyd.1
ABoyd.1Author
Associate
June 25, 2020

My bad, it seems like I didn't read enough on the MOSI MISO "idle state" litterature. SPI MOSI / MISO pins seem to idle indifferently high or low depending on the last bit sent and that shouldn't be an issue...

Thanks!