HAL_SPI_RxCpltCallback not being called after HAL_SPI_Receive_IT is being completed
hi,
I'm new in ST. I'm trying to implement SPI communication between FPGA and STM32L051R8T6 (slave).
I've initialized the spi bus in main (HAL_SPI_Init()), so that it is set to use (HAL_SPI_RxCpltCallback).
and from main i called HAL_SPI_Receive_IT (to recieve 2 bytes).
I am expecting that after the 2 bytes recive HAL_SPI_RxCpltCallback will be called and i could transmit back the data. however HAL_SPI_RxCpltCallback is not being called and it just complete the function and return to main
has anyone encountered this scenario before and could assist?