HAL Library does not support UART Rx Timeout RTOR
Hi all,
I am using STM32L433, and checked the manual that it supports rx timout for the uart. I am using cubeMX v4.22.1 with Cube L4 firmware Package v1.9.0. I try to receive unknown sized data from UART3 but i do not want to get interrupt for every byte I receive. Therefore i searched for the issue, and i found USART_RTOR, which is perfect for my needs. İ try to use it but unfortunatel HAL library does not support this timeout register duties. I try to add these lines to the init part of uart
WRITE_REG
(huart3.
Instance
->RTOR,
3
);
SET_BIT
(huart3.
Instance
->CR1, USART_CR1_RTOIE);
SET_BIT
(huart3.
Instance
->CR2, UART_RECEIVER_TIMEOUT_ENABLE);
then i observe that RTOF flag is set, good news. But i can not find any IRQ triggered when this flag is set. Therefore i can not get interrupt when the receiver timeout occurs. Does anybody have the same issue? Or am i missing something. Furthermore, does the HAL developmend tem planning to add RTOR to the library?