Question
HAL IRQ Handlers busy waiting
Posted on April 04, 2016 at 11:47
Hi @all,
I'm using HAL library V1.4 in my current project. While checking error handling functions, I came across some problems with interrupt handling in combination with FreeRTOS (https://sourceforge.net/p/freertos/discussion/382005/thread/ca400abe
/). While analyzing this problem, I found that the HAL library does busy waiting within some of the interrupt handler functions,e.g.:HAL_DMA_IRQHandler(i2c_handle)calls static HAL_StatusTypeDef I2C_WaitOnSTOPFlagUntilTimeout(I2C_HandleTypeDef *hi2c, uint32_t Timeout){ uint32_t tickstart = 0x00;->tickstart = HAL_GetTick();->while(__HAL_I2C_GET_FLAG(hi2c, I2C_FLAG_STOPF) == RESET) { /* Check if a NACK is detected */ if(I2C_IsAcknowledgeFailed(hi2c, Timeout) != HAL_OK) { return HAL_ERROR; } /* Check for the Timeout */--->if((Timeout == 0) || ((HAL_GetTick()-tickstart) > Timeout)) { hi2c->ErrorCode |= HAL_I2C_ERROR_TIMEOUT; hi2c->State= HAL_I2C_STATE_READY; /* Process Unlocked */ __HAL_UNLOCK(hi2c); return HAL_TIMEOUT; } } return HAL_OK;}In the case of an error, the calling IRQ handler blocks for 25 ms (at 1ms tick). But even without errors, I would prefer not to have busy-waiting IRQs...To circumvent this, I now would like to move the IRQ handler call into an low priority RTOS thread which is then unblocked by the IRQ.My question: Is it save to call the HAL IRQ handler functions from within normal code context instead of interrupt context? This is not only for I2C but for all peripherals.Thanks for your help!