Skip to main content
Barber.Mark
Associate III
August 18, 2015
Question

HAL I2C problems

  • August 18, 2015
  • 2 replies
  • 1025 views
Posted on August 18, 2015 at 07:18

I have been trying to use the latest HAL drivers, make thing easier once you understand their complexity. I am up to trying to get the I2C port working. i have no activity on the I2C bus at all the pins remain high all the time. If I bit bang I can get a respoonse from the slave. So the hardware is ok. i am using I2C2 on the F407VG processor

The init code is

GPIO_InitTypeDef I2C2_init;

I2C2_init.Pin=GPIO_PIN_10 | GPIO_PIN_11;

I2C2_init.Mode=GPIO_MODE_AF_OD;

I2C2_init.Pull=GPIO_PULLUP;

I2C2_init.Speed=GPIO_SPEED_LOW;

I2C2_init.Alternate=GPIO_AF4_I2C2;

HAL_GPIO_Init(GPIOB,&I2C2_init);

then

__HAL_RCC_I2C2_CLK_ENABLE();

then the I2C setup

I2C_HandleTypeDef  hi2c2;

hi2c2.Instance = I2C2;

hi2c2.Init.AddressingMode =I2C_ADDRESSINGMODE_7BIT;

hi2c2.Init.ClockSpeed=10000;

hi2c2.Init.DualAddressMode=I2C_DUALADDRESS_DISABLE;

hi2c2.Init.DutyCycle = I2C_DUTYCYCLE_16_9;

hi2c2.Init.GeneralCallMode = I2C_GENERALCALL_DISABLE;

hi2c2.Init.NoStretchMode = I2C_NOSTRETCH_DISABLE;

hi2c2.Init.OwnAddress1=0;

hi2c2.Init.OwnAddress2=0;

HAL_I2C_Init(&hi2c2);

then using the following

i2c_status=HAL_I2C_Master_Transmit(&hi2c2,208,rtcBuff,7,200);

slave address is 208 from rtcBuff 7 bytes time out 200

i get i2c_status as always being HAL_BUSY

but no bus activity. Clearly I have missed something. Any suggestions?

#i2c #stm32f407
This topic has been closed for replies.

2 replies

Nesrine M_O
Associate
August 19, 2015
Posted on August 19, 2015 at 13:15

Hi,

1. The I2C flag is busy? 

2. GPIO Clocks are enabled? 

You can try to:

1. change the IOs speed, 

2. If not search other SDA/SCL Pins, 

3. You can take a look to one I2C examples under STM32Cube_FW_F4 package, it can be very helpful.

-Syrine-

Barber.Mark
Associate III
August 31, 2015
Posted on August 31, 2015 at 03:24

Hi Thanks for the comment. I reduced the speed and the slave now responds ok.

regrads and thanks Mark