HAL_FLASHEx_Erase() fails using FreeRTOS
Hi all,
I am developing a bootloader + update system which needs FLASH pages manipulation (unlock/erase/program) from a FreeRTOS task.
The same unlock/erase code works fine if called
before
the os scheduler is launched, but fails when called from a task. What I am missing?thanks,
Adriano
MCU: Cortex L4
Firmware version: STM32Cube_FW_L4_V1.8.1
code:
int erase_partition(const uint8_t *addr)
{
int ret = HAL_OK;
uint32_t PAGEError = 0;
FLASH_EraseInitTypeDef EraseInitStruct;
HAL_FLASH_Lock();
/* Unlock the Flash to enable the flash control register access *************/
ret = HAL_FLASH_Unlock();
if (ret != HAL_OK) {
return ret;
}
/* Clear OPTVERR bit set on virgin samples */
__HAL_FLASH_CLEAR_FLAG(FLASH_FLAG_OPTVERR);
EraseInitStruct.TypeErase = FLASH_TYPEERASE_PAGES;
EraseInitStruct.Banks = FLASH_BANK_1;
EraseInitStruct.Page = get_page((uint32_t)addr);
EraseInitStruct.NbPages = APP_NUMPAGES;
ret = HAL_FLASHEx_Erase(&EraseInitStruct, &PAGEError);
if (ret != HAL_OK) {
ret = HAL_FLASH_GetError();
return ret;
}
return HAL_OK;
}