Skip to main content
westfw
Associate
January 24, 2015
Question

HAL documentation: .CHM files?

  • January 24, 2015
  • 3 replies
  • 1256 views
Posted on January 24, 2015 at 06:52

The older ''Standard Peripheral Library'' came with a really wonderful .CHM file that cross-indexed all the documentation and source code.

Is that available for the new ST Cube libraries (and the HAL in particular)?

    This topic has been closed for replies.

    3 replies

    Montassar BEN ROMDHANE_O
    Visitor II
    January 26, 2015
    Posted on January 26, 2015 at 09:54

    Hi,

    The new STM32Cube FW packages come with *.chm UM for all HAL drivers, a UM is provided for each superset RNP.

    Just take a look to the

    http://www.st.com/st-web-ui/static/active/en/st_prod_software_internet/resource/technical/software/firmware/stm32cubef4.zip

    Drivers/STM32F4xx_HAL_Driver folder.

    Regards,

    Heisenberg.

    westfw
    westfwAuthor
    Associate
    January 27, 2015
    Posted on January 27, 2015 at 06:58

    Thanks! That's exactly what I was looking for.

    However, the .chm files are not present in the STM32Cube downloads for F2, F3, L0, or L1 processor families (all of which are at v1.1 or earlier. The F0 Cube file is 1.2.0, and the F4 is 1.4.0)

    > ls -l
    
    drwxr-xr-x@ 11 staff 374 Jan 26 21:26 STM32Cube_FW_F0_V1.2.0/
    drwxr-xr-x@ 11 staff 374 Jan 26 21:44 STM32Cube_FW_F2_V1.1.0/
    drwxr-xr-x@ 10 staff 340 Oct 22 15:28 STM32Cube_FW_F3_V1.1.0/
    drwxr-xr-x@ 11 staff 374 Jan 26 21:43 STM32Cube_FW_F4_V1.4.0/
    drwxr-xr-x@ 11 staff 374 Jan 26 21:44 STM32Cube_FW_L0_V1.1.0/
    drwxr-xr-x@ 10 staff 340 Sep 4 23:06 STM32Cube_FW_L1_V1.0.0/
    > find . -name \*.chm
    ./STM32Cube_FW_F0_V1.2.0/Drivers/STM32F0xx_HAL_Driver/STM32F070xB_HAL_Driver_UM.chm
    ./STM32Cube_FW_F0_V1.2.0/Drivers/STM32F0xx_HAL_Driver/STM32F072xB_HAL_Driver_UM.chm
    ./STM32Cube_FW_F0_V1.2.0/Drivers/STM32F0xx_HAL_Driver/STM32F091xC_HAL_Driver_UM.chm
    ./STM32Cube_FW_F4_V1.4.0/Drivers/STM32F4xx_HAL_Driver/STM32F411xE_User_Manual.chm
    ./STM32Cube_FW_F4_V1.4.0/Drivers/STM32F4xx_HAL_Driver/STM32F417xx_User_Manual.chm
    ./STM32Cube_FW_F4_V1.4.0/Drivers/STM32F4xx_HAL_Driver/STM32F439xx_User_Manual.chm

    Montassar BEN ROMDHANE_O
    Visitor II
    January 28, 2015
    Posted on January 28, 2015 at 10:26

    Yes, I confirm that.

    The next versions of the STM32Cube_FW packages will include the *.chm files.

    Just keep an eye out for the next updates.

    Regards,

    Heisenberg.