Skip to main content
thannara123
Associate III
July 25, 2024
Question

HAL_DMA_XferCpltCallback function is not trigger when DMA is transfer the data

HI , am a beginner 

i am using the follwing code 

HAL_TIM_PWM_Start_DMA(&htim1, TIM_CHANNEL_1, (uint32_t *)sine_table, 20); HAL_TIMEx_PWMN_Start(&htim1, TIM_CHANNEL_1); // Start the DMA with the 180-degree phase-shifted sine wave table on channel 2 HAL_TIM_PWM_Start_DMA(&htim1, TIM_CHANNEL_2, (uint32_t *)sine_table, 20); HAL_TIMEx_PWMN_Start(&htim1, TIM_CHANNEL_2);

 

Whenver the data transfer through the DMA is completed the  HAL_DMA_XferCpltCallback function is not triggering .

why it so happen whats worng with me 

But 

void DMA2_Stream2_IRQHandler(void)

this function trigger .

 

This topic has been closed for replies.

1 reply

ST Employee
September 6, 2024

Hello @thannara123, 

Looking back at older questions, I suppose this question is answered in this thread: Solved: Re: hdma_tim1_ch1.XferCpltCallback = TransferCompl... - STMicroelectronics Community 

Could you please confirm it? 

Thank you! 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.