Associate III
December 16, 2021
Question
H725 screen flickering....
- December 16, 2021
- 2 replies
- 2150 views
I'm using the STM32H725 for development.
An image was displayed on the LCD.
There is only one screen view, and a container is placed under it, and an image is placed in the container.
The image is displayed normally, but the screen is flickering.
However, if I reduce the container size, the screen doesn't break and looks normal.
Please review which settings are strange...
Attach the project and screen video.