Question
H7 series peripheral performance in VOS2 and 3
The datasheets for the interface characteristics of each peripheral state "VOS level set to VOS1" which is the 400MHz option. But no information is given on if any of the peripherals derate if you use the slower speed and power VOS options. Would especially be interested in whether the max speed of the SPI1-3 degrade from 100MHz. I'm suspecting they might as SPI4-6 are in a different power area and only run at 50MHz.