Hi @DDeba.1
Thank you for reporting this issue and details.
AFAIK, FLASH_SALES_TYPE_Pos is not addressing position. It indicates a sort of product identification sales number to be shifted as detailed in header flash defines:
#define OB_DUAL_BANK_BASE (FLASH_R_BASE + 0x20U) /*!< Not use cmsis FLASH alias to avoid iar warning about volatile reading sequence */
#define FLASH_SALES_TYPE_Pos (24U)
#define FLASH_SALES_TYPE (0x3UL << FLASH_SALES_TYPE_Pos) /*!< 0x000001E0 */
#define FLASH_SALES_TYPE_0 (0x1UL << FLASH_SALES_TYPE_Pos) /*!< 0x01000000 */
#define FLASH_SALES_TYPE_1 (0x2UL << FLASH_SALES_TYPE_Pos) /*!< 0x02000000 */
#define FLASH_SALES_VALUE ((*((uint32_t *)PACKAGE_BASE)) & (FLASH_SALES_TYPE))
#define OB_DUAL_BANK_VALUE ((*((uint32_t *)OB_DUAL_BANK_BASE)) & (FLASH_OPTR_DUAL_BANK))
#define FLASH_BANK_NB (((FLASH_SALES_VALUE == 0U)\
|| ((FLASH_SALES_VALUE == FLASH_SALES_TYPE_0) && (OB_DUAL_BANK_VALUE == 0U)))?1U:2U)
So, it seems to be an error in the definition of the FLASH_BANK_NB macro. To be checked internally with our dedicated team (203408). Also, INDEX_PAGE macro should not be using the 2 bank.
To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.Best regards,FBL