Skip to main content
Apostolos Staridis
Associate
May 17, 2017
Question

GPS receiver for P-NUCLEO-LRWAN1

  • May 17, 2017
  • 4 replies
  • 884 views
Posted on May 17, 2017 at 18:38

Hello,

I am working with the board P-NUCLEO-LRWAN1 (

https://community.st.com/external-link.jspa?url=http%3A%2F%2Fwww.st.com%2Fen%2Fevaluation-tools%2Fp-nucleo-lrwan1.html

) for a project. I want to add a GPS receiver to that board for the purpose of that project . Can you tell me which one I should choose ? And how difficult is to get NMEA data ?

Thank you in advance

    This topic has been closed for replies.

    4 replies

    Tesla DeLorean
    Guru
    May 17, 2017
    Posted on May 17, 2017 at 18:55

    I'm using the DISCO board, but a shield like this should suffice. On the Nucleo-64 D0/D1 has some conflict with the ST-LINK VCP but you might have other pin choices

    Removing link for Duinopeak GPS Shield NEO-6M to break the moderation on this post..

    NMEA data starts automatically at 9600 8N1, connect it to a few USART input.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Tesla DeLorean
    Guru
    May 17, 2017
    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..