Solved
GPO is not working properly
- 2 replies
- 1266 views
Hi Guys I'm facing one problem in GPO side .i have try to read the input pin PA_3 and PA_2 that time i'm facing one issue .
what i'm do try to read the switch using PA_3 and PA_2 Software side i have write pull down
when i'm press the switch one PA_3 executing that loop same pa_2 but problem i have press the PA_3 switch is working Pa_2 loop and i press the pa_2 switch but is working pa_3 loop sometime is work normally
this is my code so please help