Skip to main content
MVerm.2
Associate II
Feb 6, 2021 7:23 PM UTC
Solved

GPIO pins stuck in HIGH state

Hi

I am working on a project using LL libraries and STM32F407VET6 Board.

(I have attached the main.c code here.)

The code generated by the STMCube GUI configuration tool is causing issues with two GPIOA pins (Pin 6 and 7) stuck to HIGH whenever the code runs. (When I press reset, they are OFF but as soon as program runs, they turn on again)

I removed user-specific code as much as possible still the issue persists. Also tried to pull them low using LL_GPIO_ResetOutputPin(GPIOA,L_GPIO_PIN_6|LL_GPIO_PIN_7); but no effect

These two pins are connected to two on-board user LEDs which keep glowing. Below is the GPIO function generated by STMcube.

static void MX_GPIO_Init(void)
{
 LL_GPIO_InitTypeDef GPIO_InitStruct = {0};
 
 /* GPIO Ports Clock Enable */
 LL_AHB1_GRP1_EnableClock(LL_AHB1_GRP1_PERIPH_GPIOE);
 LL_AHB1_GRP1_EnableClock(LL_AHB1_GRP1_PERIPH_GPIOC);
 LL_AHB1_GRP1_EnableClock(LL_AHB1_GRP1_PERIPH_GPIOH);
 LL_AHB1_GRP1_EnableClock(LL_AHB1_GRP1_PERIPH_GPIOA);
 LL_AHB1_GRP1_EnableClock(LL_AHB1_GRP1_PERIPH_GPIOB);
 LL_AHB1_GRP1_EnableClock(LL_AHB1_GRP1_PERIPH_GPIOD);
 
 /**/
 LL_GPIO_ResetOutputPin(GPIOA, LL_GPIO_PIN_0|LL_GPIO_PIN_1|LL_GPIO_PIN_2|LL_GPIO_PIN_3
 |LL_GPIO_PIN_4|LL_GPIO_PIN_5|LL_GPIO_PIN_6|LL_GPIO_PIN_7);
 
 /**/
 LL_GPIO_ResetOutputPin(GPIOD, LL_GPIO_PIN_0|LL_GPIO_PIN_1|LL_GPIO_PIN_2|LL_GPIO_PIN_3
 |LL_GPIO_PIN_4|LL_GPIO_PIN_5|LL_GPIO_PIN_6|LL_GPIO_PIN_7);
 
 /**/
 LL_GPIO_ResetOutputPin(GPIOE, LL_GPIO_PIN_0|LL_GPIO_PIN_1);
 
 /**/
 GPIO_InitStruct.Pin = LL_GPIO_PIN_2|LL_GPIO_PIN_4|LL_GPIO_PIN_5|LL_GPIO_PIN_6
 |LL_GPIO_PIN_7|LL_GPIO_PIN_8|LL_GPIO_PIN_9|LL_GPIO_PIN_10
 |LL_GPIO_PIN_11|LL_GPIO_PIN_12|LL_GPIO_PIN_13|LL_GPIO_PIN_14
 |LL_GPIO_PIN_15;
 GPIO_InitStruct.Mode = LL_GPIO_MODE_ANALOG;
 GPIO_InitStruct.Pull = LL_GPIO_PULL_NO;
 LL_GPIO_Init(GPIOE, &GPIO_InitStruct);
 
 /**/
 GPIO_InitStruct.Pin = LL_GPIO_PIN_3;
 GPIO_InitStruct.Mode = LL_GPIO_MODE_INPUT;
 GPIO_InitStruct.Pull = LL_GPIO_PULL_NO;
 LL_GPIO_Init(GPIOE, &GPIO_InitStruct);
 
 /**/
 GPIO_InitStruct.Pin = LL_GPIO_PIN_13|LL_GPIO_PIN_14|LL_GPIO_PIN_15|LL_GPIO_PIN_0
 |LL_GPIO_PIN_1|LL_GPIO_PIN_2|LL_GPIO_PIN_3|LL_GPIO_PIN_4
 |LL_GPIO_PIN_5|LL_GPIO_PIN_6|LL_GPIO_PIN_7|LL_GPIO_PIN_8
 |LL_GPIO_PIN_9|LL_GPIO_PIN_12;
 GPIO_InitStruct.Mode = LL_GPIO_MODE_ANALOG;
 GPIO_InitStruct.Pull = LL_GPIO_PULL_NO;
 LL_GPIO_Init(GPIOC, &GPIO_InitStruct);
 
 /**/
 GPIO_InitStruct.Pin = LL_GPIO_PIN_0|LL_GPIO_PIN_1|LL_GPIO_PIN_2|LL_GPIO_PIN_3
 |LL_GPIO_PIN_4|LL_GPIO_PIN_5|LL_GPIO_PIN_6|LL_GPIO_PIN_7;
 GPIO_InitStruct.Mode = LL_GPIO_MODE_OUTPUT;
 GPIO_InitStruct.Speed = LL_GPIO_SPEED_FREQ_LOW;
 GPIO_InitStruct.OutputType = LL_GPIO_OUTPUT_PUSHPULL;
 GPIO_InitStruct.Pull = LL_GPIO_PULL_NO;
 LL_GPIO_Init(GPIOA, &GPIO_InitStruct);
 
 /**/
 GPIO_InitStruct.Pin = LL_GPIO_PIN_0|LL_GPIO_PIN_1|LL_GPIO_PIN_2|LL_GPIO_PIN_10
 |LL_GPIO_PIN_11|LL_GPIO_PIN_12|LL_GPIO_PIN_13|LL_GPIO_PIN_14
 |LL_GPIO_PIN_15|LL_GPIO_PIN_3|LL_GPIO_PIN_4|LL_GPIO_PIN_5
 |LL_GPIO_PIN_6|LL_GPIO_PIN_7|LL_GPIO_PIN_8|LL_GPIO_PIN_9;
 GPIO_InitStruct.Mode = LL_GPIO_MODE_ANALOG;
 GPIO_InitStruct.Pull = LL_GPIO_PULL_NO;
 LL_GPIO_Init(GPIOB, &GPIO_InitStruct);
 
 /**/
 GPIO_InitStruct.Pin = LL_GPIO_PIN_8|LL_GPIO_PIN_9|LL_GPIO_PIN_10|LL_GPIO_PIN_11
 |LL_GPIO_PIN_12|LL_GPIO_PIN_13|LL_GPIO_PIN_14|LL_GPIO_PIN_15;
 GPIO_InitStruct.Mode = LL_GPIO_MODE_ANALOG;
 GPIO_InitStruct.Pull = LL_GPIO_PULL_NO;
 LL_GPIO_Init(GPIOD, &GPIO_InitStruct);
 
 /**/
 GPIO_InitStruct.Pin = LL_GPIO_PIN_8|LL_GPIO_PIN_11|LL_GPIO_PIN_12|LL_GPIO_PIN_15;
 GPIO_InitStruct.Mode = LL_GPIO_MODE_ANALOG;
 GPIO_InitStruct.Pull = LL_GPIO_PULL_NO;
 LL_GPIO_Init(GPIOA, &GPIO_InitStruct);
 
 /**/
 GPIO_InitStruct.Pin = LL_GPIO_PIN_9|LL_GPIO_PIN_10;
 GPIO_InitStruct.Mode = LL_GPIO_MODE_ALTERNATE;
 GPIO_InitStruct.Speed = LL_GPIO_SPEED_FREQ_VERY_HIGH;
 GPIO_InitStruct.OutputType = LL_GPIO_OUTPUT_PUSHPULL;
 GPIO_InitStruct.Pull = LL_GPIO_PULL_NO;
 GPIO_InitStruct.Alternate = LL_GPIO_AF_7;
 LL_GPIO_Init(GPIOA, &GPIO_InitStruct);
 
 /**/
 GPIO_InitStruct.Pin = LL_GPIO_PIN_0|LL_GPIO_PIN_1|LL_GPIO_PIN_2|LL_GPIO_PIN_3
 |LL_GPIO_PIN_4|LL_GPIO_PIN_5|LL_GPIO_PIN_6|LL_GPIO_PIN_7;
 GPIO_InitStruct.Mode = LL_GPIO_MODE_OUTPUT;
 GPIO_InitStruct.Speed = LL_GPIO_SPEED_FREQ_LOW;
 GPIO_InitStruct.OutputType = LL_GPIO_OUTPUT_PUSHPULL;
 GPIO_InitStruct.Pull = LL_GPIO_PULL_NO;
 LL_GPIO_Init(GPIOD, &GPIO_InitStruct);
 
 /**/
 GPIO_InitStruct.Pin = LL_GPIO_PIN_0|LL_GPIO_PIN_1;
 GPIO_InitStruct.Mode = LL_GPIO_MODE_OUTPUT;
 GPIO_InitStruct.Speed = LL_GPIO_SPEED_FREQ_LOW;
 GPIO_InitStruct.OutputType = LL_GPIO_OUTPUT_PUSHPULL;
 GPIO_InitStruct.Pull = LL_GPIO_PULL_NO;
 LL_GPIO_Init(GPIOE, &GPIO_InitStruct);
 
 LL_GPIO_ResetOutputPin(GPIOA, LL_GPIO_PIN_0|LL_GPIO_PIN_1|LL_GPIO_PIN_2|LL_GPIO_PIN_3|LL_GPIO_PIN_4|LL_GPIO_PIN_5|LL_GPIO_PIN_6|LL_GPIO_PIN_7); //Added by me
}

Please help. Full code is attached herewith.

Thanks in advance

This topic has been closed for replies.
Vangelis Fortounas
Associate II
Feb 6, 2021 9:00 PM UTC

Hello

>> These two pins are connected to two on-board user LEDs which keep glowing

If Leds are connected to anode is normal to remain ON.

Try to pull High PA6, to observe the difference.

2 replies

Vangelis Fortounas
Associate II
Feb 6, 2021 9:00 PM UTC

Hello

>> These two pins are connected to two on-board user LEDs which keep glowing

If Leds are connected to anode is normal to remain ON.

Try to pull High PA6, to observe the difference.

MVerm.2
MVerm.2Author
Associate II
Feb 7, 2021 7:13 AM UTC

Thank you very much. I never thought this can also be a possibility since most of the boards use LEDs connected between Pin and GND.