Skip to main content
Associate III
September 14, 2023
Question

GPIO HAL pointer at function argument

  • September 14, 2023
  • 6 replies
  • 1662 views

Hi, i m reading the general HAL GPIO file, what does the 2 pointers here do? can anyone kindly advise? i see a lot of STM header and device file with these... 

void HAL_GPIO_Init(GPIO_TypeDef *GPIOx, GPIO_InitTypeDef *GPIO_Init)
{
uint32_t position = 0x00U;
uint32_t iocurrent;
uint32_t temp;

EXTI_Core_TypeDef *EXTI_CurrentCPU;

#if defined(DUAL_CORE) && defined(CORE_CM4)

EXTI_CurrentCPU = EXTI_D2; /* EXTI for CM4 CPU */

#else
EXTI_CurrentCPU = EXTI_D1; /* EXTI for CM7 CPU */
#endif

.....

This topic has been closed for replies.

6 replies

TDK
September 14, 2023

GPIOx is a pointer to the GPIO port, e.g. GPIOA.

GPIO_Init is a pointer to the initialization structure, which holds in the information on which pins you want configured and how to configure them.

 

"If you feel a post has answered your question, please click ""Accept as Solution""."
Pavel A.
September 14, 2023

Why you don't ask what is EXTI_Core? :)

Associate III
September 15, 2023

yes, i would like to know whats  EXTI_Core and EXTI_CurrentCPU too...Anyone can kinldy advise?

TDK
September 18, 2023

Pretty sure he was joking...

You can look up these things on your own. Function definitions, structures, HAL examples all exist.

"If you feel a post has answered your question, please click ""Accept as Solution""."
Pavel A.
September 18, 2023

Thank you Tim :)