Skip to main content
Associate III
January 9, 2024
Question

GPIO_EXTI

  • January 9, 2024
  • 4 replies
  • 1427 views

Hi people,

    I just work on a Dali project and trying to learn from the demo library I am getting some error can anyone PLEASE help me how to proceed.

I am trying in STM32G0

I am getting error as EXTI.Instruture undeclared i tried EXTI.Instruct but still its showing error  'NVIC_InitStructure' undeclared 

hOW CAN I DECLARE THAT FUNCTIONS

 

 

 

void receive_tick(void)
{
 // Because of the structure of current amplifier, input has
 // to be negated
 actual_val = get_DALIIN();
 tick_count++;

 // edge detected
 if(actual_val != former_val)
 {
 switch(bit_count)
 {
 case 0:
 if (tick_count > 2)
 {
 tick_count = 0;
 bit_count = 1; // start bit
 }
 break;
 case 17: // 1st stop bit
 if(tick_count > 6) // stop bit error, no edge should exist
 flag = ERR;
 break;
 default: // other bits
 if(tick_count > 6)
 {
 if(bit_count < 9) // store bit in address byte
 {
 address |= (actual_val << (8-bit_count));
 }
 else // store bit in data byte
 {
 dataByte |= (actual_val << (16-bit_count));
 }
 bit_count++;
 tick_count = 0;
 }
 break;
 }
 }else // voltage level stable
 {
 switch(bit_count)
 {
 case 0:
 if(tick_count==8) // too long start bit
 flag = ERR;
 break;
 case 17:
 // First stop bit
 if (tick_count==8)
 {
 if (actual_val==0) // wrong level of stop bit
 {
 flag = ERR;
 }
 else
 {
 bit_count++;
 tick_count = 0;
 }
 }
 break;
 case 18:
 // Second stop bit
 if (tick_count==8)
 {
 flag = NO_ACTION;

 //enable EXTI
 EXTI_InitStructure.EXTI_Line = EXTI_LINE_6;
 EXTI_InitStructure.EXTI_Mode = EXTI_MODE_INTERRUPT;
 EXTI_InitStructure.EXTI_Trigger = EXTI_TRIGGER_FALLING;
 EXTI_InitStructure.EXTI_LineCmd = ENABLE;
 EXTI_Init(&EXTI_InitStructure);

 DataReceivedCallback(address,dataByte);
 }
 break;
 default: // normal bits
 if(tick_count==10)
 { // too long delay before edge
 flag = ERR;
 }
 break;
 }
 }
 former_val = actual_val;
 if(flag==ERR)
 {
 flag = NO_ACTION;
 //enable EXTI
 EXTI_InitStructure.EXTI_Line = EXTI_LINE_6;
 EXTI_InitStructure.EXTI_Mode = 'EXTI_MODE_INTERRUPT';
 EXTI_InitStructure.EXTI_Trigger = EXTI_TRIGGER_FALLING;
 EXTI_InitStructure.EXTI_LineCmd = ENABLE;
 EXTI_Init(&EXTI_InitStructure);
 }
}

 

 

 

This topic has been closed for replies.

4 replies

TDK
January 9, 2024

A search on Github turns on this:

typedef struct
{
 uint32_t EXTI_Line; /*!< Specifies the EXTI lines to be enabled or disabled.
 This parameter can be any combination of @ref EXTI_Lines */
 
 EXTIMode_TypeDef EXTI_Mode; /*!< Specifies the mode for the EXTI lines.
 This parameter can be a value of @ref EXTIMode_TypeDef */

 EXTITrigger_TypeDef EXTI_Trigger; /*!< Specifies the trigger signal active edge for the EXTI lines.
 This parameter can be a value of @ref EXTITrigger_TypeDef */

 FunctionalState EXTI_LineCmd; /*!< Specifies the new state of the selected EXTI lines.
 This parameter can be set either to ENABLE or DISABLE */ 
}EXTI_InitTypeDef;

 

Not sure that'll help if you don't know how to define structures. Where did you get this code anyway?

"If you feel a post has answered your question, please click ""Accept as Solution""."
SRAM.11Author
Associate III
January 9, 2024

Yes I found this in drivers but i am not sure why these used

if(flag==ERR)
 {
 flag = NO_ACTION;
 //enable EXTI
 EXTI_InitStructure.EXTI_Line = EXTI_LINE_6;
 EXTI_InitStructure.EXTI_Mode = 'EXTI_MODE_INTERRUPT';
 EXTI_InitStructure.EXTI_Trigger = EXTI_TRIGGER_FALLING;
 EXTI_InitStructure.EXTI_LineCmd = ENABLE;
 EXTI_Init(&EXTI_InitStructure);
 }

 I got is from STM32F1 DALI slave library

AScha.3
Super User
January 9, 2024

Hi,

If you generate the code with CubeIDE , (?)

just define the pins you use for exti and in NVIC choose the INT priority.  Then -> generate code -> and init functions are there.

If you feel a post has answered your question, please click on " Best Answer ".
waclawek.jan
Super User
January 9, 2024

This is probably based on SPL, which is an older library no longer supported by ST. There's no SPL for 'G0.

You should try to understand the functionality and then reproduce it on the 'G0, rather than just trying to port it blindly.

JW