Skip to main content
Associate III
February 26, 2025
Question

GPDMA Queues & Nodes

Hello, 

 

Does someone have information, project, whatever that can help me understand how do the Queues and Nodes work and interact with each other? 

 

My STM32 has two ADCs, ADC1 & ADC4, and i want to trigger both of them to read values comming from multiple potentiomenters with a timer configured in output compare mode. 

 

The problem is that i have to configure a linkedlist with a Queue and a Node and if i configure two nodes the values of the ADCs seen through the live expression get stuck at 0.

 

Any help is welcomed ...

 

 

This topic has been closed for replies.

1 reply

Amel NASRI
ST Technical Moderator
April 22, 2025

Hi @Marc3 ,

Just seeing your question now, so I think that the knowledge article How to configure the linked list mode in STM32CubeMX should answer your questions about GPDMA linked list on STM32U5.

My answer may be late for you, but it can be useful for others having similar question as yours.

-Amel

To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.