Skip to main content
sheng yang
Senior
January 22, 2024
Question

get hardfault when do division func on stm32g070 with gcc cross compile tool

  • January 22, 2024
  • 5 replies
  • 2036 views

my cross compile tool version: 

▸ arm-none-eabi-gcc -v Using built-in specs. COLLECT_GCC=arm-none-eabi-gcc COLLECT_LTO_WRAPPER=/home/red/.local/gcc-arm-none-eabi-10-2020-q4-major/bin/../lib/gcc/arm-none-eabi/10.2.1/lto-wrapper Target: arm-none-eabi Configured with: /mnt/workspace/workspace/GCC-10-pipeline/jenkins-GCC-10-pipeline-48_20201124_1606180641/src/gcc/configure --target=arm-none-eabi --prefix=/mnt/workspace/workspace/GCC-10-pipeline/jenkins-GCC-10-pipeline-48_20201124_1606180641/install-native --libexecdir=/mnt/workspace/workspace/GCC-10-pipeline/jenkins-GCC-10-pipeline-48_20201124_1606180641/install-native/lib --infodir=/mnt/workspace/workspace/GCC-10-pipeline/jenkins-GCC-10-pipeline-48_20201124_1606180641/install-native/share/doc/gcc-arm-none-eabi/info --mandir=/mnt/workspace/workspace/GCC-10-pipeline/jenkins-GCC-10-pipeline-48_20201124_1606180641/install-native/share/doc/gcc-arm-none-eabi/man --htmldir=/mnt/workspace/workspace/GCC-10-pipeline/jenkins-GCC-10-pipeline-48_20201124_1606180641/install-native/share/doc/gcc-arm-none-eabi/html --pdfdir=/mnt/workspace/workspace/GCC-10-pipeline/jenkins-GCC-10-pipeline-48_20201124_1606180641/install-native/share/doc/gcc-arm-none-eabi/pdf --enable-languages=c,c++ --enable-plugins --disable-decimal-float --disable-libffi --disable-libgomp --disable-libmudflap --disable-libquadmath --disable-libssp --disable-libstdcxx-pch --disable-nls --disable-shared --disable-threads --disable-tls --with-gnu-as --with-gnu-ld --with-newlib --with-headers=yes --with-python-dir=share/gcc-arm-none-eabi --with-sysroot=/mnt/workspace/workspace/GCC-10-pipeline/jenkins-GCC-10-pipeline-48_20201124_1606180641/install-native/arm-none-eabi --build=x86_64-linux-gnu --host=x86_64-linux-gnu --with-gmp=/mnt/workspace/workspace/GCC-10-pipeline/jenkins-GCC-10-pipeline-48_20201124_1606180641/build-native/host-libs/usr --with-mpfr=/mnt/workspace/workspace/GCC-10-pipeline/jenkins-GCC-10-pipeline-48_20201124_1606180641/build-native/host-libs/usr --with-mpc=/mnt/workspace/workspace/GCC-10-pipeline/jenkins-GCC-10-pipeline-48_20201124_1606180641/build-native/host-libs/usr --with-isl=/mnt/workspace/workspace/GCC-10-pipeline/jenkins-GCC-10-pipeline-48_20201124_1606180641/build-native/host-libs/usr --with-libelf=/mnt/workspace/workspace/GCC-10-pipeline/jenkins-GCC-10-pipeline-48_20201124_1606180641/build-native/host-libs/usr --with-host-libstdcxx='-static-libgcc -Wl,-Bstatic,-lstdc++,-Bdynamic -lm' --with-pkgversion='GNU Arm Embedded Toolchain 10-2020-q4-major' --with-multilib-list=rmprofile,aprofile Thread model: single Supported LTO compression algorithms: zlib gcc version 10.2.1 20201103 (release) (GNU Arm Embedded Toolchain 10-2020-q4-major)

And My Final link config as:

[1/1] arm-none-eabi-g++ -nostartfiles -nostdlib --specs=nosys.specs -Xlinker -print-memory-usage -Xlinker --sort-section=alignment obj/kernel/core/core.tos_barrier.o obj/kernel/core/core.tos_binary_heap.o obj/kernel/core/core.tos_bitmap.o obj/kernel/core/core.tos_char_fifo.o obj/kernel/core/core.tos_completion.o obj/kernel/core/core.tos_countdownlatch.o obj/kernel/core/core.tos_event.o obj/kernel/core/core.tos_global.o obj/kernel/core/core.tos_mail_queue.o obj/kernel/core/core.tos_message_queue.o obj/kernel/core/core.tos_mmblk.o obj/kernel/core/core.tos_mmheap.o obj/kernel/core/core.tos_mutex.o obj/kernel/core/core.tos_pend.o obj/kernel/core/core.tos_priority_mail_queue.o obj/kernel/core/core.tos_priority_message_queue.o obj/kernel/core/core.tos_priority_queue.o obj/kernel/core/core.tos_ring_queue.o obj/kernel/core/core.tos_robin.o obj/kernel/core/core.tos_rwlock.o obj/kernel/core/core.tos_sched.o obj/kernel/core/core.tos_sem.o obj/kernel/core/core.tos_stopwatch.o obj/kernel/core/core.tos_sys.o obj/kernel/core/core.tos_task.o obj/kernel/core/core.tos_tick.o obj/kernel/core/core.tos_time.o obj/kernel/core/core.tos_timer.o obj/kernel/osal/cmsis_os/cmsis_os.cmsis_os.o obj/kernel/hal/tos_hal_armv6m_gcc.o obj/kernel/arch/arm/arm-v6m/common/common.tos_cpu.o obj/kernel/arch/arm/arm-v6m/common/common.tos_fault.o obj/kernel/arch/arm/arm-v6m/cortex-m0/gcc/cortex-m0.port_c.o obj/kernel/arch/arm/arm-v6m/cortex-m0/gcc/port_s.o obj/platform/vendor_bsp/st/CMSIS/Device/ST/STM32G0xx/Source/Templates/platform.system_stm32g0xx.o obj/board/XYJ_STM32G070CBTX/APP/hello_world/startup_stm32g070xx.o obj/board/XYJ_STM32G070CBTX/APP/hello_world/APP.main.o obj/board/XYJ_STM32G070CBTX/APP/hello_world/HAL.stm32g0xx_it.o obj/platform/vendor_bsp/st/STM32G0xx_HAL_Driver/Src/HAL.stm32g0xx_hal_uart.o obj/platform/vendor_bsp/st/STM32G0xx_HAL_Driver/Src/HAL.stm32g0xx_hal_uart_ex.o obj/platform/vendor_bsp/st/STM32G0xx_HAL_Driver/Src/HAL.stm32g0xx_hal_dma.o obj/platform/vendor_bsp/st/STM32G0xx_HAL_Driver/Src/HAL.stm32g0xx_hal_rcc.o obj/platform/vendor_bsp/st/STM32G0xx_HAL_Driver/Src/HAL.stm32g0xx_hal_rcc_ex.o obj/platform/vendor_bsp/st/STM32G0xx_HAL_Driver/Src/HAL.stm32g0xx_hal_pwr.o obj/platform/vendor_bsp/st/STM32G0xx_HAL_Driver/Src/HAL.stm32g0xx_hal_pwr_ex.o obj/platform/vendor_bsp/st/STM32G0xx_HAL_Driver/Src/HAL.stm32g0xx_hal_gpio.o obj/platform/vendor_bsp/st/STM32G0xx_HAL_Driver/Src/HAL.stm32g0xx_hal_cortex.o obj/board/XYJ_STM32G070CBTX/BSP/Src/BSP.mcu_init.o obj/board/XYJ_STM32G070CBTX/BSP/Src/BSP.gpio.o obj/board/XYJ_STM32G070CBTX/BSP/Src/BSP.bsp_usart.o obj/board/XYJ_STM32G070CBTX/BSP/Src/BSP.usart.o obj/platform/vendor_bsp/st/STM32G0xx_HAL_Driver/Src/vendor_bsp_hal.stm32g0xx_hal.o -T /home/red/LearnProjects/ChipAdaptation/board/XYJ_STM32G070CBTX/LEDsingle.ld -L/home/red/.local/gcc-arm-none-eabi-10-2020-q4-major/arm-none-eabi/lib/thumb/v6-m/nofp -lgcc -Wl,-Map=LEDsingle.map -o LEDsingle.elf && arm-none-eabi-objcopy -O binary LEDsingle.elf LEDsingle.bin && arm-none-eabi-objcopy -O ihex LEDsingle.elf LEDsingle.hex && arm-none-eabi-size LEDsingle.elf 

And when I use gdb to debug, I found I will get in Hardfault_Handler, and the stack backtrace as:

(gdb) bt

#0 HardFault_Handler () at ../board/XYJ_STM32G070CBTX/APP/hello_world/stm32g0xx_it.c:89

#1

#2 0x08008ff8 in ?? ()

#3 0x08003ca2 in cpu_init () at ../kernel/arch/arm/arm-v6m/common/tos_cpu.c:81

the cpu_init func is just as: 

k_cpu_cycle_per_tick = TOS_CFG_CPU_CLOCK / k_cpu_tick_per_second;

it's equa with k_cpu_cycle_per_tick = 16000000 / 1000; 

I wonder how could this happen, I build this on stm32g070cb chip.

w

This topic has been closed for replies.

5 replies

Tesla DeLorean
Guru
January 22, 2024

Make sure it's building for CM0 core. No divide instruction, done with library code.

Check if dividing by zero

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
sheng yang
Senior
January 23, 2024

1. I build this with cflags

arm-none-eabi-gcc -MMD -MF obj/platform/vendor_bsp/st/STM32G0xx_HAL_Driver/Src/HAL.stm32g0xx_hal_uart.o.d -DSTM32G070xx -I../kernel/arch/arm/arm-v6m/common/include -I../kernel/arch/arm/arm-v6m/cortex-m0/gcc -I../kernel/core/include -I../kernel/hal/include -I../kernel/osal/cmsis_os -I../kernel/pm/include -I../board/XYJ_STM32G070CBTX/TOS-CONFIG -I../platform/vendor_bsp/st/CMSIS/Device/ST/STM32G0xx/Include -I../platform/vendor_bsp/st/CMSIS/Include -I../platform/vendor_bsp/st/CMSIS/Core/Include -I../platform/vendor_bsp/st/STM32G0xx_HAL_Driver/Inc -I../board/XYJ_STM32G070CBTX/BSP/Inc -O2 -g -fno-builtin -fno-strict-aliasing -fdiagnostics-color=always -fshort-enums -mcpu=cortex-m0plus -mthumb -Wa,-mimplicit-it=thumb -std=c99 -MP -MD -Wno-misleading-indentation -c ../platform/vendor_bsp/st/STM32G0xx_HAL_Driver/Src/stm32g0xx_hal_uart.c -o obj/platform/vendor_bsp/st/STM32G0xx_HAL_Driver/Src/HAL.stm32g0xx_hal_uart.o

as you can see here are flags with  ``-mcpu=cortex-m0plus -mthumb``. and I use -lgcc library to link with divide library code.

2. I debug with gdb step there no dividing by zero,

I do as below :

abc = abc / 1000;

can still get fault.

Tesla DeLorean
Guru
January 23, 2024

Decode the registers and code that's specifically faulting.

If you get the faulting PC, identify that in the .MAP and .LST files.

Ideally have a Hard Fault Handler that dumps these things.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
sheng yang
Senior
January 25, 2024

Final I found the mistake, there are two factors in my project:

1. I lost -mcpu=cortex-m0plus and -mthumb flags in final link process so link with wrong libgcc.a, this is the root cause.

2. I set uart1 handler enable early but the uart init func is wrong, and I wonder why this will hand cpu,:frowning_face: