Question
Genration of sine wave using DAC of Nucleo-H743zi2 development board
Hello,
I am using DAC module of STM32H743ZI2 micro controller to generate sine wave of 8KHz frequency I am using Timer2 for this setting using APB1 bus of 150MHz and prescaler of 74 and ARR register of 1.
>>The issue I am facing is jitter in the output wave form like +/-50Hz deviation from 8KHz.
>>I want also sine wave whose frequency varies from 5KHz to 20KHz in steps of 0.1Hz with a delay of 100ms between each frequency step with low jitter is that possible