Question
Generating 100us timer base & cnt (STM32F205)
Posted on November 04, 2014 at 13:46
1. I have STM32F205 running at 120Mhz with external 16Mhz crystal.
Prefetch , Data & Instruction buffer on. timer is clocked by 60Mhz2. task is to toggle 10 pins with a base count of 100us.i.e User will enter number in multiple of 100us & I have to toggle the pins.3. I have timer base of 100us & accordingly I am toggled the pins. In interrupt only 10 variables are incremented. So ISR is very small.4. System works fine initially but on long run (1 hour or so), I saw some latency keep on adding. 5. This probably due to small time base i.e 100us. It adds jitter & theoretically Cortex-M3 core should always be able to service an interrupt request within 15 cycles . Is it due to these cycles which accumulate over period of time & generate error.6. Any possible solution/advise/technical point