Question
Generate .hex for FlashLoaderDemonstrator with EWARM 6.70.1.5794
Posted on February 08, 2015 at 23:36
Hello,
I'm using IAR EWARM 6.70.1.5794 for developping a firmware on a STM32F107VCT6. I use a ST LINK V2 for debug. Now i would like generate an hex or bin file for downloading the file without ST-LIN V2 but with Flash Loader Demonstrator in bootloader mode. I have tried Project -> Options -> Output Converter -> Generate additional output file / Intel extended but when i try to load the file with Flash Loader demonstrator, i have an error : ''unable to load this file...'' I have although tried to unselect ''include debug information in output'' but that's the same problem =( Anyone have an idea to solve this? Thanks #flash-demonstrator-iar-hex