Skip to main content
Associate
May 16, 2024
Question

Generate a checksum

I need to generate a checksum of data from X address(FLASH) to Y address (FLASH). and write at last 4 bytes of FLASH memory in "xyz" section. 

When I say calculate checksum, I mean addition of all given data bytes from X address(FLASH) to Y address (FLASH).

Can we do it at compilation time ?

 

 

This topic has been closed for replies.

1 reply

Lead II
May 17, 2024

If you write a script (e.g. in Python) which can read your generated ELF or BIN file - sure.
You have to provide this script and add it as a post-compile step.

The compiler itself does not do. But you are free to add this as a step after code generation. And what and how to do: it is only you (therefore you had to write a script post-processing the compile results).