Skip to main content
Tobe
Senior III
Mar 15, 2024 1:23 PM UTC
Solved

G431 will run (somewhat) with debugger, but not on its own.

I have made a prototype, and it runs as just after upload. But when i just turn on the power, it wont. It does not matter if the st-linkv3 ist connected or not. When i reset it, via the NRST pin, it also wont run.

I already used the HSE and HSI, and checked on a nucleo, that my code is working (it does).

I dont know how i further can investigate this. The level of NRST is clean and the level is good.

This topic has been closed for replies.
Tobe
TobeBest answer
Senior III
Mar 15, 2024 2:49 PM UTC

It works:

I had to set nSWBOOT0 to 0. See picture attached.

Thanks a lot.

5 replies

mƎALLEm
ST Technical Moderator
Mar 15, 2024 1:27 PM UTC

Hello,

What about Boot pin? connected to VDD or GND?

See for example this thread: https://community.st.com/t5/stm32-mcus-products/stm32h723zgt6-will-not-reboot-after-powering-off/m-p/650457

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
Tobe
TobeAuthor
Senior III
Mar 15, 2024 2:41 PM UTC

Neither: It is connected to RX of a CAN chip. See attached the waveforms.

pink is Boot0 pin, blue is 3.3V of STM

 

mƎALLEm
ST Technical Moderator
Mar 15, 2024 2:45 PM UTC

Hello,

Neither: It is connected to RX of a CAN chip. See attached the waveforms.

 

Sorry.. I didn't catch that point!  How did you connect Boot pin? which CAN chip? could you please share schematics?


pink is Boot0 pin, blue is 3.3V of STM


Pink signal is rising. It should be connected to the ground. Why BOOT pin voltage is changing?

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
Tesla DeLorean
Guru
Mar 15, 2024 1:29 PM UTC

BOOTx pins or settings?

Get a USART working very early in the Reset Handler so you can express signs-of-life. Could perhaps use GPIO/LEDs at as simpler level. Have Hard Fault and Error Handlers output actionable data.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Tobe
TobeAuthorBest answer
Senior III
Mar 15, 2024 2:49 PM UTC

It works:

I had to set nSWBOOT0 to 0. See picture attached.

Thanks a lot.