Skip to main content
Tobe
Senior III
Apr 5, 2024 6:54 AM UTC
Solved

G431 Config of input interrupt prevents timer 8 from working.

This is one that baffles me:

I set up Timer 8, and everything haasworking perfect. Then i did set up interrupt on some pins, and then the PWM signal on timer 8 stopped working.

This is what i did, so the Timer 8 stopped working:

Edit: Only with the pull UP resistor the problem does not appear.

 

 

 

 

 

	my_GPIO_InitStruct.Pin = GPIO_PIN_0 | GPIO_PIN_1 | GPIO_PIN_2;
	my_GPIO_InitStruct.Mode = GPIO_MODE_IT_RISING_FALLING;
	my_GPIO_InitStruct.Pull = GPIO_NOPULL;
	HAL_GPIO_Init(GPIOC, &my_GPIO_InitStruct);

 

 

 

 

 

This is how i setup Timer 8:

 

 

 

 

 

	// **************** PWM *********************
	// PC6-8
	// PC10-12
	my_GPIO_InitStruct.Pin = 	GPIO_PIN_6 |
								GPIO_PIN_7 |
								GPIO_PIN_8 |
								GPIO_PIN_10 |
								GPIO_PIN_11 |
								GPIO_PIN_12;
	my_GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
	my_GPIO_InitStruct.Pull = GPIO_NOPULL;
	my_GPIO_InitStruct.Speed = GPIO_SPEED_LOW;
	HAL_GPIO_Init(GPIOC, &my_GPIO_InitStruct);
	// Alternative function HIGH register
	GPIOC->AFR[0] |= (	GPIO_AFRL_AFSEL6_2 | 	// AF4 (all)
						GPIO_AFRL_AFSEL7_2);
	// Alternative function LOW register
	GPIOC->AFR[1] |= (	GPIO_AFRH_AFSEL8_2 |	// AF4 (all)
						GPIO_AFRH_AFSEL10_2 |
						GPIO_AFRH_AFSEL11_2 |
						GPIO_AFRH_AFSEL12_2);

SET_BIT(RCC->APB2ENR, RCC_APB2ENR_TIM8EN); 		// Enable TIM8 clock

	CLEAR_REG(TIM8->AF1);	// Disable BKIN input
	CLEAR_REG(TIM8->AF2);

	SET_BIT(TIM8->CR1, 	TIM_CR1_ARPE | 				// preload enable
						TIM_CR1_CMS_1 // center aligned up/down (interrupt on counting up - for ADC trigger only?)
						);

	//TODO: check entries again for pwm
	SET_BIT(TIM8->CR2, TIM_CR2_MMS2_3 | TIM_CR2_MMS2_2); // tim_oc4refc or tim_oc6refc rising edges generate pulses on	tim_trgo2 for ADC trigger

	//TIMx_ARR -1 ist max counter
	WRITE_REG(TIM8->ARR, PWM_WIDTH); // Counter TOP

	// Prescaler TIMx_PSC

	WRITE_REG(TIM8->CCR1, DUTY_TO_PWM(15));	// compare value 1
	WRITE_REG(TIM8->CCR2, DUTY_TO_PWM(30));	// compare value 2
	WRITE_REG(TIM8->CCR3, DUTY_TO_PWM(80));	// compare value 3

	WRITE_REG(TIM8->CCR4, PWM_WIDTH - ADC_TRIG_PRE_COUNT);	// compare value 4 (ADC trigger)

	//The UEV update event can be disabled by software by setting the UDIS bit in the TIMx_CR1


	SET_BIT(TIM8->CCMR1, 	TIM_CCMR1_OC1M_2 | TIM_CCMR1_OC1M_1	| // pwm output compare polarity channel 1 and 2 (pwm mode 1)
							TIM_CCMR1_OC2M_2 | TIM_CCMR1_OC2M_1	);
	SET_BIT(TIM8->CCMR1, 	TIM_CCMR1_OC1PE | TIM_CCMR1_OC2PE); 	// preload enable ccr 1 + 2
	// Default is OUTPUT !!!
	// CC1S = 0 > channel output (CC1 as OUTPUT)

	SET_BIT(TIM8->CCMR2, 	TIM_CCMR2_OC3M_2 | TIM_CCMR2_OC3M_1	| // pwm output compare polarity channel 3 and 4 (pwm mode 1)
							TIM_CCMR2_OC4M_2 | TIM_CCMR2_OC4M_1	);
	SET_BIT(TIM8->CCMR2, 	TIM_CCMR2_OC3PE | TIM_CCMR2_OC4PE); 	// preload enable ccr 3 + 4


	SET_BIT(TIM8->CCER, TIM_CCER_CC1E | TIM_CCER_CC2E | TIM_CCER_CC3E); 	// compare 1 + 2 + 3 output enable
	SET_BIT(TIM8->CCER, TIM_CCER_CC1NE | TIM_CCER_CC2NE | TIM_CCER_CC3NE); 	// compare 1 + 2 + 3 complementary output enable
	// TODO: CC1P: Capture/compare 1 output polarity ????

	// Load all register via Update event
	SET_BIT(TIM8->EGR , 1); // (UG)



	SET_BIT(TIM8->CR1, TIM_CR1_CEN); //Counter enable
	SET_BIT(TIM8->BDTR, TIM_BDTR_MOE); // Connect signals to outputs (When CCxE and CCxNE are set - see also OSSR and OSSI)
	WRITE_REG(TIM8->SR, 0); 	// Clear any int flags

 

 

 

 

 

 

I think it has something to do with the interrupt. But i dont have set up the interrupt for it yet. But when debugging, it wont go into an error handler. When i activate the pullup, then it works fine, or if i change it to just input mode.

When debugging, it does NOT get stuck somewhere in the code.

This topic has been closed for replies.
Tobe
TobeBest answer
Senior III
Apr 5, 2024 5:03 PM UTC

After carefully debugging i found the cause:

I have an interrupt on another pin with number 2, so the interrupt routine is called, which by chance was deactivating timer 8.

Jeeeez.

7 replies

waclawek.jan
Super User
Apr 5, 2024 8:30 AM UTC

Read out and check/compare-to-working/post content of TIM and relevant GPIO registers.

JW

Tobe
TobeAuthor
Senior III
Apr 5, 2024 10:16 AM UTC

I dont know really what would be relevant. Im thinking it has something to do with the execution of a interrupt.

I edited my original post.

waclawek.jan
Super User
Apr 5, 2024 12:33 PM UTC

You said, TIM8 stopped working when you set TIM1.

So you want to observe difference of registers content before and after setting TIM1 (i.e. between the working and non-working case).

JW

Tobe
TobeAuthor
Senior III
Apr 5, 2024 1:52 PM UTC

Amongst a few other register from timer 8, there is one crucial bit not set:

STM32G431xx/TIM8/CR1/CEN:0x0

But how can that happen, wenn i just change a pull up/down resistor???

And HOW can it affect settings that will be set in the future and also from a different timer?

Tobe
TobeAuthorBest answer
Senior III
Apr 5, 2024 5:03 PM UTC

After carefully debugging i found the cause:

I have an interrupt on another pin with number 2, so the interrupt routine is called, which by chance was deactivating timer 8.

Jeeeez.