Skip to main content
ezrab
Associate III
October 5, 2010
Question

full speed micro

  • October 5, 2010
  • 4 replies
  • 933 views
Posted on October 05, 2010 at 09:39

what is the full speed system clock i can

achieve with stm32-discovery?

and how?

now i work with 8Mhz cristal.

    This topic has been closed for replies.

    4 replies

    Tesla DeLorean
    Guru
    October 5, 2010
    Posted on October 05, 2010 at 16:35

    It is documented to be 24 MHz, you need to configure the PLL, and you can use the AHB/APB1/APB2 with no scaling (ie at 24 MHz). The flash will also run at this speed without wait states.

    The PLL would be set to (HSE / 2) * 6

    If you are using the standard library you can select the speed in system_stm32f10x.c by changing a #define, or program it yourself, either way review the code in the ST firmware library (at the address printed on the board) to see how to configure the clocks.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    ezrab
    ezrabAuthor
    Associate III
    October 6, 2010
    Posted on October 06, 2010 at 08:10

    thanks for the replay .

    i used this configuration:

     RCC->APB2ENR |=0x14;

     RCC->CR = (uint32_t)0x00000000;

     RCC->CFGR=0x4000005;

     RCC->CR=0x1090000;

    but still i cant get any higher then 8Mhz.

    why?

    joa
    Visitor II
    October 6, 2010
    Posted on October 06, 2010 at 10:18

    As far as I can see from your magic numbers you don't select the PLL as system clock. You can try something like this (it seems to work but I don't know if it's the correct way to do it)

        //// Configure system clock PLL*3 driven by  external high speed

        //// oscillator (8 MHz crystall) 24MHz

        // Turn on high speed external oscillator

        RCC->CR |= RCC_CR_HSEON;

        // Wait until it's ready

        while ((RCC->CR & RCC_CR_HSERDY) == 0)

            ;

        // Select PREDIV1 as PLL source and sett PLL mul to 3 (set bit 0)

        // for 8*3 = 24 MHz

        RCC->CFGR |= RCC_CFGR_PLLSRC | RCC_CFGR_PLLMULL_0;

        // Start PLL

        RCC->CR |= RCC_CR_PLLON;

        // Wait until it's ready

        while ((RCC->CR & RCC_CR_PLLRDY) == 0)

            ;

        // Select PLL as system clock

        RCC->CFGR |= RCC_CFGR_SW_PLL;

        // Here we can check if PLL is used, and maybe disable HSI

        // Disable HSI

        RCC->CR &= ~RCC_CR_HSION;

    (Is there some kind of code tags one can use?)

    ezrab
    ezrabAuthor
    Associate III
    October 6, 2010
    Posted on October 06, 2010 at 10:30

    thank you very much it works :)