Skip to main content
ralf2
Associate
Sep 12, 2014 10:47 AM UTC
Question

FSMC WR behavior

Posted on September 12, 2014 at 12:47

In a nearly ready project i wanted to add some more types of TFT displays. Now i�ve got one with an SSD1298 controller, for which well working init-code is available. I connected it in well known manner to the FSMC and it happened NOTHING...Studying the documantation of the display in precision i see: WR ist Write signal, active at Rising edge !!! So my problem is that the FSMC provides an active low Signal. Is it possible to change this behavior? I would not like to put additional hardware to the ready project. Has someone an idea? Thanks

#fsmc-stm32-wr-line
This topic has been closed for replies.