Skip to main content
kisnemeth
Associate
April 23, 2010
Question

FSMC and SRAM Example halts

  • April 23, 2010
  • 2 replies
  • 611 views
Posted on April 23, 2010 at 10:12

FSMC and SRAM Example halts

    This topic has been closed for replies.

    2 replies

    Nickname12657_O
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 13:48

    Hi,

    You can refer to our latest Firmware published on web, we already include template files for Ride and run it on your board. I suspect that FSMC area is not configured or initialized in the right way.

    Cheers,

    STOne-32.

    kisnemeth
    kisnemethAuthor
    Associate
    May 17, 2011
    Posted on May 17, 2011 at 13:48

    Hi STOne-32,

    The latest v3.3.0 of firmware solved this problem. I used the old version becouse I'd had to implement a new function into an old project which used the v2.x.x firmware. Now I have to update the full project to v3.x.x. But at least it works!

    Thank You,

    Robert