Skip to main content
Associate II
December 6, 2023
Solved

FreeRTOS STM32H743ZI FPU Assembler Error

Hi there,
I’m trying to compile a project using the STM32H743ZI2 Nucleo board with STM32CUBE Framework with FreeRTOS with PlatformIO.

The project can be found here:
Zafeer_FreeRTOSFromGroundUp/PlatformIO/17_WorkingWithQueueSets at main · ZafeerAbbasi/Zafeer_FreeRTOSFromGroundUp (github.com)

But basically, I’m using an extra script to add flags:

Import( “env” )

flags = [
    "-mcpu=cortex-m7",
    "-mfloat-abi=hard",
    "-mfpu=fpv5-d16",
    "-mthumb",
    "-u _printf_float",
    "-DDEBUG",
    "--specs=nano.specs",
    "-march=armv7e-m",
    "-std=gnu11",
    "-g3"
]
env.Append(CCFLAGS=flags, LINKFLAGS=flags, ASFLAGS=flags)

However I keep getting the following errors:

…\Local\Temp\ccTwSuW0.s: Assembler messages:
…\Local\Temp\ccTwSuW0.s:330: Error: selected processor does not support vstmdbeq r0!,{s16-s31}' in Thumb mode ...\Local\Temp\ccTwSuW0.s:332: Error: instruction not allowed in IT block -- stmdb r0!,{r4-r11,r14}’
…\Local\Temp\ccTwSuW0.s:352: Error: selected processor does not support vldmiaeq r0!,{s16-s31}' in Thumb mode ...\Local\Temp\ccTwSuW0.s:354: Error: instruction not allowed in IT block -- msr psp,r0’
*** [.pio\build\nucleo_h743zi\libe54\Source\portable\GCC\ARM_CM4F\port.o] Error 1

The exact instructions can be found in port.c of FreeRTOS Kernel:

void xPortPendSVHandler( void )
{
    /* This is a naked function. */

    __asm volatile
    (
    "   mrs r0, psp                         \n"
    "   isb                                 \n"
    "                                       \n"
    "   ldr r3, pxCurrentTCBConst           \n" /* Get the location of the current TCB. */
    "   ldr r2, [r3]                        \n"
    "                                       \n"
    "   tst r14, #0x10                      \n" /* Is the task using the FPU context?  If so, push high vfp registers. */
    "   it eq                               \n"
    "   vstmdbeq r0!, {s16-s31}             \n"
    "                                       \n"
    "   stmdb r0!, {r4-r11, r14}            \n" /* Save the core registers. */
    "   str r0, [r2]                        \n" /* Save the new top of stack into the first member of the TCB. */
    "                                       \n"
    "   stmdb sp!, {r0, r3}                 \n"
    "   mov r0, %0                          \n"
    "   msr basepri, r0                     \n"
    "   dsb                                 \n"
    "   isb                                 \n"
    "   bl vTaskSwitchContext               \n"
    "   mov r0, #0                          \n"
    "   msr basepri, r0                     \n"
    "   ldmia sp!, {r0, r3}                 \n"
    "                                       \n"
    "   ldr r1, [r3]                        \n" /* The first item in pxCurrentTCB is the task top of stack. */
    "   ldr r0, [r1]                        \n"
    "                                       \n"
    "   ldmia r0!, {r4-r11, r14}            \n" /* Pop the core registers. */
    "                                       \n"
    "   tst r14, #0x10                      \n" /* Is the task using the FPU context?  If so, pop the high vfp registers too. */
    "   it eq                               \n"
    "   vldmiaeq r0!, {s16-s31}             \n"
    "                                       \n"
    "   msr psp, r0                         \n"
    "   isb                                 \n"
    "                                       \n"
    #ifdef WORKAROUND_PMU_CM001 /* XMC4000 specific errata workaround. */
        #if WORKAROUND_PMU_CM001 == 1
    "           push { r14 }                \n"
    "           pop { pc }                  \n"
        #endif
    #endif
    "                                       \n"
    "   bx r14                              \n"
    "                                       \n"
    "   .align 4                            \n"
    "pxCurrentTCBConst: .word pxCurrentTCB  \n"
    ::"i"(configMAX_SYSCALL_INTERRUPT_PRIORITY)
    );
}

I’m not too experienced but any help would be greatly appreciated!

This topic has been closed for replies.
rockybalboa__Best answer
Associate II
December 6, 2023

The solution was based on PlatformIO platform.ini file, basically instead of:

extra_scripts = add_hardfloat.py
I used:
extra_scripts = pre:add_hardfloat.py
and that did the trick!

( Also I used the CM7 Port instead of the CM4 port, S/O to @RomainR. for pointing that out!

4 replies

RomainR.
ST Employee
December 6, 2023

Hello @rockybalboa__ 

I'm not familliar with PlateformIO IDE, but in errors you get, it seems you are using port.c of FreeRTOS Kernel for CM4. As STM32H7 is a CM7, you should use adequate FreeRTOS port.c for CM7.

Regards,

Romain,   

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Associate II
December 6, 2023

Thank you for pointing that out, it really did help!

rockybalboa__AuthorBest answer
Associate II
December 6, 2023

The solution was based on PlatformIO platform.ini file, basically instead of:

extra_scripts = add_hardfloat.py
I used:
extra_scripts = pre:add_hardfloat.py
and that did the trick!

( Also I used the CM7 Port instead of the CM4 port, S/O to @RomainR. for pointing that out!
RomainR.
ST Employee
December 6, 2023

Thank you @rockybalboa__ 

Does it mean "pre:add_hardfloat.py" is a typo ?

Regards.

Romain,

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.