Solved
Free UART on P-L496G-CELL02 board?
We are using the P-L496G-CELL02 demo board and want to connect an external device through an UART.
Is there (for example USART1) accessible for external connection? Which ports are connected to the Arduino compatible interface? Is there an UART aviable?
Or are there schematics of the board aviable?
Regards,
Michael