Skip to main content
Liviu Ionescu
Associate III
August 2, 2016
Question

Free Development Tools: GNU ARM Eclipse

  • August 2, 2016
  • 19 replies
  • 3268 views
Posted on August 02, 2016 at 18:05

Please add GNU ARM Eclipse, with a reference to http://gnuarmeclipse.github.io, to the list of free, open source, development environments with strong support for STM32 devices.

Regards,

Liviu

#free-development-ide-gnu-arm
    This topic has been closed for replies.

    19 replies

    Liviu Ionescu
    Associate III
    August 13, 2016
    Posted on August 13, 2016 at 11:27

    any moderator reading this post?

    Amel NASRI
    ST Technical Moderator
    August 15, 2016
    Posted on August 15, 2016 at 17:36

    Hi Liviu Ionescu,

    Thanks for your contribution in the STM32 forum. 

    Do you mean to add GNU ARM Eclipse in the sticky discussion available in this forum?

    I will check what can be done, if possible please provide more details on the supported devices...

    -Mayla-

    To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.
    Liviu Ionescu
    Associate III
    August 26, 2016
    Posted on August 26, 2016 at 09:37

    > Do you mean to add GNU ARM Eclipse in the sticky discussion available in this forum?

    yes, Mayla, please add the following:

    * GNU ARM Eclipse (http://gnuarmeclipse.github.io) - supports 

    all STM32 devices based on ARM Cortex-M0, M0+, M3, M4, and M7 cores. Runs on Windows, GNU/Linux and macOS. Advanced debugging features, including emulator. Completely free, completely open source.

    Thank you,

    Liviu

    Liviu Ionescu
    Associate III
    September 8, 2016
    Posted on September 08, 2016 at 08:18

    Mayla? did you see this message?

    Liviu Ionescu
    Associate III
    October 3, 2016
    Posted on October 04, 2016 at 00:05

    Mayla? Anyone else moderating this forum?

    marcello2
    Visitor II
    October 5, 2016
    Posted on October 05, 2016 at 10:52

    I think that no one should ignore the wonderful work by Liviu Ionescu for the GNU ARM developers community.

    Chapeau

    Liviu Ionescu
    Associate III
    October 6, 2016
    Posted on October 06, 2016 at 11:25

    Thank you, @ferri.marcello.

    Can anyone help me contact the moderators?

    Liviu

    AvaTar
    Senior III
    October 6, 2016
    Posted on October 06, 2016 at 13:24

    There is this ''Contact moderator'' menu there:

    0690X00000602czQAA.jpg

    However, I would not be surprised if it didn't work ...

    Liviu Ionescu
    Associate III
    October 10, 2016
    Posted on October 10, 2016 at 18:40

    > There is this ''Contact moderator'' menu 

    I did this, twice, but it was of no use. :(

    any other suggestions?

    AvaTar
    Senior III
    October 11, 2016
    Posted on October 11, 2016 at 08:26

    As said - I'm not surprised it doesn't work.

    This is the most pathetic attempt of a ''forum webpage'' I ever came across.

    > any other suggestions?

     

    Aside from bumping this thread up, perhaps trying to contact ST engineers directly ?

    I guess they are too busy to fix their Cube mess. Adding support for another toolchain (however good), seem lined up far behind fixing GUI bugs, fixing code generation bugs, and fixing support for newer MCUs.

    Just my personal impression ...