Skip to main content
Theo Spalinger
Visitor II
August 15, 2017
Question

Framebuffer for STemWin Application in internal RAM

  • August 15, 2017
  • 1 reply
  • 592 views
Posted on August 15, 2017 at 12:15

I want to build my own hardware with a stm32f769 (with 512 kBytes internal RAM)

I want to use the STemWin. 

The example 'STemWin_HelloWorld' supplied with the STM32F769I_EVAL Kit uses the external SDRAM.

Due to cost savings, i want to place the framebuffer to the internal RAM of the 

stm32f769 controller.

Is this possible?

Is anyone experienced in this issue?

Thanks

    This topic has been closed for replies.

    1 reply

    Amel NASRI
    Technical Moderator
    August 16, 2017
    Posted on August 16, 2017 at 18:14

    Hi

    Spalinger.Theo.002

    ‌,

    Almost the same question asked in

    https://community.st.com/0D50X00009XkXS6SAN

    , but regarding STM32F4 device.

    A solution was suggested by

    Horbach.Markus

    ‌ there.

    -Amel

    To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.