Skip to main content
Associate III
June 27, 2024
Solved

Frame buffer in FMC SDRAM on FMC display with same pins

Hello, I have a quick question. I'm wondering if I can put the frame buffer in SDRAM connected via FMC when I use FMC LCD controller to controll Display that uses the same address pins of FMC.

This topic has been closed for replies.
mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
September 7, 2024

Hello,

You can do that but think about the contention on FMC interface and the performance: read/write to the memory and to the LCD.

You need to do some performance tests.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.

1 reply

mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
September 7, 2024

Hello,

You can do that but think about the contention on FMC interface and the performance: read/write to the memory and to the LCD.

You need to do some performance tests.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.