Question
four uarts on stm32L433?
Posted on September 05, 2017 at 22:05
Is it possible to get four USART/UART devices at once on the STM32L433 in a 64-pin package? I need one UART for input, one for output, one for external logging, and USART1 for debugging.
Is this doable? I've used CubeMX to try various configurations, and I end up short of the goal. I'll also need an ADC and a PWM or DAC, and DMA on at least the input device would be nice.Suggestions?