Skip to main content
sonia
Associate
December 7, 2015
Question

For the Chip STM32L151RBH6, how to make EEPROM writting doesn't halt MCU?

  • December 7, 2015
  • 0 replies
  • 418 views
Posted on December 07, 2015 at 04:02

For the Chip STM32L151RBH6, we have only 1 bank, EEPROM writting halt the MCU. I make a test program to repeatedly write EEPROM. Use the code like below to write EEPROM:

*(__IO uint32_t *)addr = data;

100 times repeated write consumed 673ms: 6.72ms once.

50 times repeated write consumed 336ms:6.72ms once

The Reference Manual addressed: ''This function can be executed from any memory. If it is from the same bank the program is stalled for one Tprog.'' So I tried to implemente the write from Ram function. The result didn't change great.

1. 50 times consumed 324ms, 6.47ms

2. 100 times 663ms, 6.63ms

    This topic has been closed for replies.