Skip to main content
kashubadmitry
Associate III
Nov 16, 2016 8:44 AM UTC
Question

For STM32F407 how to set PLL as the source of SYSCLK and to see it on pin MCO1 o

Posted on November 16, 2016 at 09:44

Hi! I wrote program for STM32F407, where I set PLL as the source of SYSCLK and want to see it on pin MCO1.

The program is:

#include ''stm32f4xx.h''

uint32_t i, temp;

int main()

{

//config clock

RCC->CR=RCC_CR_HSION;

while (!(RCC->CR&RCC_CR_HSIRDY));

RCC->APB1ENR=RCC_APB1ENR_PWREN;

PWR->CR|= PWR_CR_VOS;

RCC->PLLCFGR=RCC_PLLCFGR_PLLSRC_HSI;

RCC->PLLCFGR|=0x00000F08;//n=60, m=8, hs=8 MHz, p=2

RCC->CR|=RCC_CR_PLLON;

while (!(RCC->CR&RCC_CR_PLLRDY));

FLASH->ACR|=FLASH_ACR_LATENCY_5WS;

RCC->CFGR|= (RCC_CFGR_PPRE2_DIV2|RCC_CFGR_PPRE1_DIV4);

RCC->CFGR|= RCC_CFGR_SW_PLL;

//enable gpio, usart6, mac

RCC->AHB1ENR=RCC_AHB1ENR_GPIOAEN;//vkl takt port

//config type GPIO

GPIOA->MODER|=GPIO_MODER_MODER8_1;

//GPIOA->OSPEEDR=GPIO_OSPEEDER_OSPEEDR8;

RCC->CFGR|=RCC_CFGR_MCO1;

while (1);

}

Impulses on MCO1 are wrong!

What must I do to solve the problem?

 

Thank You!

    This topic has been closed for replies.

    2 replies

    waclawek.jan
    Super User
    Nov 16, 2016 11:07 AM UTC
    Posted on November 16, 2016 at 12:07

    How wrong?

    What instrument do you use to verify it?

    Why did you comment out the pin's speed setting?

    Did you observe the PLL input/output frequency limits?

    JW
    Tesla DeLorean
    Guru
    Nov 16, 2016 3:16 PM UTC
    Posted on November 16, 2016 at 16:16

    I'm not going to wade into the register mess of OR'ing everything together...

    Clean concise SPL example..

    void ClockMCO(void)
    {
    GPIO_InitTypeDef GPIO_InitStructure;
    /* Enable GPIOs clocks */
    RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOA, ENABLE);
    /* Enable SYSCFG clock */
    RCC_APB2PeriphClockCmd(RCC_APB2Periph_SYSCFG, ENABLE);
    /* Configure MCO (PA8) */
    GPIO_InitStructure.GPIO_Pin = GPIO_Pin_8;
    GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz;
    GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
    GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
    GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL ;
    GPIO_Init(GPIOA, &GPIO_InitStructure);
    GPIO_PinAFConfig(GPIOA, GPIO_PinSource8, GPIO_AF_MCO); // Should be default
    /* Output PLL/2 clock on MCO pin (PA8), you could try /1 if below 100 MHz */
    RCC_MCO1Config(RCC_MCO1Source_PLLCLK, RCC_MCO1Div_2);
    }

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..