Skip to main content
AN.16
Visitor II
December 28, 2018
Question

For an STM32F427 / STM32F429 MCU is UART supported with 0.5 Stop Bit and DMA enabled configuration???

  • December 28, 2018
  • 2 replies
  • 682 views

I am using an STM32F429FI Nucleo board, and not able to communicate over UART with the confiiguration having 0.5 Stop bits and DMA being enabled.

Is this a valid configuration? Data sheet suggests use of 0.5 Stop bits with SmartCard mode does it mean it is not supported for regular mode of UART communication

This topic has been closed for replies.

2 replies

S.Ma
Principal
December 28, 2018

DMA gets request from peripheral to read/write data bytes. The stop bits are not involved.

Beware smartcard needs USART and not UART. Find a working example to look at the HW registers setting in debug mode and compare.

Tesla DeLorean
Guru
December 28, 2018

General rule is that if it works in polled mode it can also be done with DMA.

Doesn't work how? Can out output a pattern, and does it look correct on scope or analyzer? If not show or describe how it is wrong..​

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..