Skip to main content
Visitor II
Aug 19, 2025 9:51 AM UTC
Solved

FMC SDRAM design recommendations (STM32F446)

Hello,

I am designing a board with a STM32F446 connected to an IS42S16160H SDRAM through the FMC interface.

Could you please provide ST’s official recommendations regarding the use of series resistors on FMC lines?

  • Typical values (22–33 Ω)?

  • Any ST guideline or application note available?

Thanks,

Rihem

This topic has been closed for replies.
ELABI.1
ELABI.1Best answer
ST Technical Moderator
Aug 21, 2025 10:57 AM UTC

Hi @Rihem_,

You can take a look at these guidelines for the FMC interface in this Application Note AN4488:

ELABI1_0-1755773391207.png

 

In these guidelines, it is not recommended to use series resistors if you ensure that the transmission line (trace) on the PCB has a controlled characteristic impedance around 50 ohms.

However, if you need further optimization for the signal integrity, you can use series resistors. To determine the exact value, you need to perform a simulation using the IBIS models of the STM32F4.

For this purpose, you can refer to Application Note AN4803, which contains an example showing how to perform a simulation with HyperLynx on an MCU for SDRAM memory using the FMC controller, specifically in section 5.1 HyperLynx simulation with SDRAM.

This is the link to download the IBIS models for STM32F4 to use in your simulation

Thanks.

ELABI.1

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

1 reply

ELABI.1
ELABI.1Best answer
ST Technical Moderator
Aug 21, 2025 10:57 AM UTC

Hi @Rihem_,

You can take a look at these guidelines for the FMC interface in this Application Note AN4488:

ELABI1_0-1755773391207.png

 

In these guidelines, it is not recommended to use series resistors if you ensure that the transmission line (trace) on the PCB has a controlled characteristic impedance around 50 ohms.

However, if you need further optimization for the signal integrity, you can use series resistors. To determine the exact value, you need to perform a simulation using the IBIS models of the STM32F4.

For this purpose, you can refer to Application Note AN4803, which contains an example showing how to perform a simulation with HyperLynx on an MCU for SDRAM memory using the FMC controller, specifically in section 5.1 HyperLynx simulation with SDRAM.

This is the link to download the IBIS models for STM32F4 to use in your simulation

Thanks.

ELABI.1

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.