Skip to main content
Visitor II
March 19, 2025
Question

FMC initialising and RTC desactivation

 Dear All, 

I designed a HMI board with STM32F767 and QSPI NOR flash and MT48LC16M SDRAM with external OSC 8MHz and MC-306 32.768 KHz.

Approximately I tested more than 100 PCs of this board and all work without any problem. 

but during this week in some new boards, I saw when I initialise FMC, the RTC does not work anymore. even with RTC again initialising, it still doesn’t work and need to get restarted or power off. 
I also tested with internal LSI but nothing changes. I also connected V BAT to VDD the problem is still there. 
funny thing that this software works in many of these boards, but some of them have exactly the same problem.
I also removed the SDRAM and NoR flash chips, but again had same problem. 
Any body have had this problem? 

This topic has been closed for replies.

1 reply

mƎALLEm
ST Technical Moderator
April 2, 2025

Hello,

Not obvious to tell what the problem is as there is no relation between FMC and RTC. You need to start a debug session and check where it fails in your code. Check all the return HAL APIs especially those of the RTC it may indicate the fail.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.